2017-12-20 9:21 AM
Hello guys! Help me please... I have problems with the CubeMX, can not generator code create project((( Operating system Linux Mint 18
Solved! Go to Solution.
2017-12-21 1:06 PM
guys, isolved the problem. Reinstalled java 8, for some reason not enough one dependencies
Now working good!Has also installed new program from STM STM32CubeProgrammer, now all works on Linux!
Thanks a lot, dear
Turvey.Clive.002
andDAHMEN.IMEN
.new version Java 8:
java version '1.8.0_151'
Java(TM) SE Runtime Environment (build 1.8.0_151-b12) Java HotSpot(TM) 64-Bit Server VM (build 151-b12, mixed mode)2017-12-21 7:09 AM
Hello,
Could you please provide more details about the version used?
Please ensure to use the last CubeMx version.
Best Regads
Imen
2017-12-21 8:52 AM
Especially version and state of Java being used.
2017-12-21 11:16 AM
Hello!
java -version
java version '1.8.0_144'Java(TM) SE Runtime Environment (build 8.0.5.0 - pxa6480sr5-20170905_01(SR5))IBM J9 VM (build 2.9, JRE 1.8.0 Linux amd64-64 Compressed References 20170901_363591 (JIT enabled, AOT enabled)J9VM - d56eb84JIT - tr.open_20170901_140853_d56eb84OMR - b033a01)JCL - 20170823_01 based on Oracle jdk8u144-b01//-----------------------------------------------------------------------------------------------------------------------
STM32CubeMX version 4.23
2017-12-21 1:06 PM
guys, isolved the problem. Reinstalled java 8, for some reason not enough one dependencies
Now working good!Has also installed new program from STM STM32CubeProgrammer, now all works on Linux!
Thanks a lot, dear
Turvey.Clive.002
andDAHMEN.IMEN
.new version Java 8:
java version '1.8.0_151'
Java(TM) SE Runtime Environment (build 1.8.0_151-b12) Java HotSpot(TM) 64-Bit Server VM (build 151-b12, mixed mode)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.