STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC Issue on STM32H747I-DISCO

Hello,After trying almost everything I found online, I’m posting here for help.I’m working with an STM32H747I-DISCO board, aiming to exchange data via USB CDC with Windows. I’ve configured the .ioc for USB CDC device (FS or HS) on the Cortex M7 core....

StatusQ by Associate
  • 1527 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H573RIV6 VDDUSB

Hello,  I am using the STM32H573RIV6 for my project and would like to use the USB interface. However, according to the datasheet, the VDDUSB pin is not available for the VFQFPN68 package. Does this mean the USB feature is not available for the STM32H...

HarshaK by Associate II
  • 1782 Views
  • 4 replies
  • 2 kudos

Counting pulses with STM32G474

Hi, In my STM32G474 project, I'm receiving a signal consisting of a burst of pulses, with a relatively long idle period before the next burst. I'm trying to setup a system where I use timers to count the pulses, and a slave timer to detect the idle p...

HaraldAnt by Associate II
  • 1737 Views
  • 2 replies
  • 1 kudos

STM32F072 PWM One pulse

HelloNeed help, need to set PWM in a one pulse mode, so that at start timer there would be a low level output for a time equal to value of CCRx, after compare the output would be change to a high level and would remain so after overflow and stopping ...

1.png
peit by Associate II
  • 3174 Views
  • 8 replies
  • 0 kudos

Resolved! STM32H755 Dual Debug Startup Problem

Hi community,I have a problem that other people have also raised and I'd be grateful for help.I followed AN5361 and I watched this STM video on the same topic. First thing to mention is that the video and doc have different advice about whether the C...

bramble_0-1740832043277.png bramble_7-1740832218457.png bramble_9-1740832308142.png bramble_4-1740832152320.png
bramble by Senior
  • 2067 Views
  • 4 replies
  • 1 kudos

Resolved! NUCLEO-H753ZI: Communication with PC

I'm trying to use my NUCLEO-H753ZI board to send some message to my PC using UART. I read from the data sheet that USART3 is connected to the ST-LINK for the Virtual COM Port (VCP), and USART3 can directly transmit messages to the PC. However, in the...

Screenshot 2025-03-06 at 21.54.57.png
doronzzz by Associate II
  • 2273 Views
  • 3 replies
  • 0 kudos

Tutorial of SPL2LL converter

Posted on July 17, 2017 at 15:49Hello ,  It's a good news , ST finaly develop a application to migrate from SPL to LL ,there's any tutorial please , how to use this convertor , what's the exeption .... Best regards #migrate #migrate-from-stmf4-to-st...

Resolved! STM32U5 HSE Crystal

I'm currently at schematic stage designing a board based around the STM32U5G9ZJT6Q. The PCB will be produced and assembled by JLCPCB, so I had a look for a HSE crystal they have in stock and found this:https://jlcpcb.com/partdetail/YangxingTech-X3225...

STM32U5_HSE.png
AMars.4 by Associate III
  • 1664 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.