STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F446RE Nucleo and IDW01M1

Posted on January 30, 2018 at 10:25Hello everyone, to begin with i have little experience in ARM embedded world besides Arduino and ESP32 boards. Recently i stepped into STM32 Nucleo programming. My tools is STM32CubeMX and KEIL IDE. Since this poin...

Restart DMA - STM32F767

Posted on January 30, 2018 at 11:35Hello.I have question. How to restart DMA?I have this init function:&sharpdefine DMA_RX_BUFF_SIZE            64         uint8_t dma_rx_buff[DMA_RX_BUFF_SIZE];void MX_UART5_Init(void){ /* Enable CLOCK for GPIO */ LL...

Timer 1 Channel 4 -Compare interrupt problem

Posted on January 30, 2018 at 16:00Trouble getting capture compare ( no output ) interrupt to function correctly.First.. I'm using HAL, with the free Keil MDK. Maybe this is the problem, so first question:Is there any simple Keil examples that like ...

Is it possible to wakeup the STM32 using USB data?

Posted on January 30, 2018 at 17:54Hi, we are sleeping the STM32F072xB using PWR_EnterSTOPMode() and waking on various GPIO for button press, etc.  Is it possible to wake on a USB message?  Is there an app note or example on this?  Does anybody know...

Is it possible to wakeup the STM32 using USB data?

Posted on January 30, 2018 at 17:48Hi, we sleep the STM32F072xB using PWR_EnterSTOPMode() and currently wake from some GPIO like button press.  We do have a USB connection up and I'm wondering if the other side could wake us with a USB message.  Is ...

Resolved! STM32F429I-DISC1 Rev. C Changes/Specifications/Documents

Posted on January 30, 2018 at 16:13I just ordered and received REV C of this board, all of the files online seem to indicate they apply to REV B of the board, is anyone aware of the changes or has access to the appropriate files? #stm32f429i-disc1

evan by Associate II
  • 1289 Views
  • 2 replies
  • 0 kudos

DMA stream configuration in HAL Cube

Posted on January 30, 2018 at 17:12 Hello, I am trying to setting up a template project to work with the SPI and DMA triggered by a timer using the STM32F746ZG. The configuration I need to program is the one in the attached image. Need to t...

DMA2D Config

Posted on January 17, 2018 at 12:14I am trying to create a project which uses a display. I have created a project on stm32cube with LTDC and DMA2D enabled. I can store bitmaps in the flash then display them using the LTDC functions. I have got an ex...

STM32 Sleep

Posted on January 29, 2018 at 13:02What is the best way to put STM32L0 micro-controllers to sleep for limited time duration(preferably using RTC)?#stm32l0 #stm32-sleep

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.