2018-01-17 3:14 AM
I am trying to create a project which uses a display. I have created a project on stm32cube with LTDC and DMA2D enabled. I can store bitmaps in the flash then display them using the LTDC functions. I have got an example project working on a stm32f7 device where you can overlay bitmaps using the DMA2D. I have tried to get this working on my project but with no luck, as I need to overlay lots of small bitmaps stored in the flash quickly.
If I set the background colour to white I get activty on all the display lines in the LTDC functions. If I set the background colour to black there is only activity on the clock hysnc etc, which is what you would expect.
I then tried to use the DMA2D to send some data to the display but there is no activity. I have tried to use the example code for the DMA2D but it doesnt seem to be running. I have enabled the clock. Is there any way of debugging it/common errors made when using the DMA2D.
2018-01-19 6:02 AM
Has anyone got an ideas? Been trying again but still with no luck.
2018-01-30 8:10 AM
Is there any tutorials that I can follow please? I have searched online and there is nothing definitive for implementing it
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.