2018-01-30 9:00 AM
I am attempting to use CDC Host libraries but am having trouble. I have not been able to find an example in Cube.
My setup
I have used the CDC Device libraries with great success in the past to provide a terminal interface to a PC. Do I need a special cable to from the 3240G FS to the 496G FS connector. I’m currently using a cable that was supplied with the 3240G board. It has a rectangular connector on one end that fits the 3240G FS connector (CN8) and a D shaped connector on the other end that fits the L496G FS connector (CN8). When I connect the boards with this cable the host libraries on the 3240G do not see the connection.
I could also really use some help on how to transmit and receive using the Host CDC libraries. No example and nothing apparent.
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.