STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

CubeMX STM32L433CC ETR2 Input bug?

Posted on March 06, 2017 at 17:48 Hi When TIM2 of this device is configured according to the screenshot, the following code will be generated: void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle) { GPIO_InitTypeDef GPIO_InitStruct;...

Losing color depth

Posted on February 12, 2018 at 01:45I've been working on a simple UI library for my project.I'm using the stm32F7 with LTDC configured to RGB888 color space.Whilst I was writing a color gradient function, I noticed that my gradients looked 'choppy'L...

0690X00000604NDQAY.jpg

F767 micro SD card freezes

Posted on February 12, 2018 at 09:40I'm experiencing random freezing of the micro SD card on a custom board, running the STM32F767II.During read operations, occasionally communications is lost to the card and the driver code will experience repeatin...

STM32L151 touch sesing

Posted on February 12, 2018 at 07:03Hi all,I want to enable touch sensing in L151. I used Cube to configure and when I go to configuration tab and click on TS, I get a pop-up showing 'Cube does not support configuration of this IP mode. You can conf...

SP1ML , AND XCUBE spirit1 library

Posted on November 20, 2017 at 14:04 hello every body , now i could establish connection with my sp1ml using uart and i can communicate between two sp1ml just with hyperterminal using AT COMMANDS after downloading the standart firmware !! now i n...

0690X0000060PFfQAM.jpg

How to get the PDM data by DFSDM module at STM32L4xx

Posted on February 09, 2018 at 02:17I use DFSDM(at STM32L471RE) to record voice. the human's voice is record OK. but I can not record the heartbeat voice. it is about 500Hz.So I want to read the PDM data and analyze at PC.How to get the PDM data?I t...

hgyxbll by Associate II
  • 2259 Views
  • 4 replies
  • 0 kudos

769disco and 746disco - what is the direction?

Posted on February 09, 2018 at 06:53   ST is to be complimented for three specific design improvements apparent in the 769disco.  FIrst, it actually has a connector to the display, rather than the LCD cable being soldered directly to the board, as i...

STM32F103RBT6 doesn't run after ROP option set

Posted on February 09, 2018 at 01:13HiI am using ST-LINK to program a STM32F103RBT6.  I program it and the unit runs - then I set option bytes via the menu for readout protection and the unit stops.  Power cycle et al does not recover.  Are there ot...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.