2018-02-15 10:25 PM
Hello,
i am working with the STM32L073x on the evaluation board STM32L073VZ and the Nucleo-L073RZ and I want to figure out the functionality of the USB DFU Update via internal bootloader.
As descibed in several application notes I already did the following steps:
After choosing the desired *.dfu file and pressing 'Upgrade' The tool shows 'Erasing' for a very short time, followed by 'Target 00: Upgrade successful !' (Operation Time only one second)
But there is no data transmission, the Transfererd Data size remains at 0KB.
If I connect another eval boad ( STM32F4xx Disco) the procedure works fine. So the environment seems to be ok, there must be a dependecy to the STM32L073.
Does anyone have a usefull advice?
Thanks
2018-02-26 7:33 AM
Same here with my custom boards and nucleo Boards
2018-02-26 9:00 AM
I'll link to the other thread here
https://community.st.com/0D50X00009XkdtVSAR
DAHMEN.IMEN
st.mcu
benahmed.mohamed
perhaps ST can open/provide the source for some of these utilities that seem to have been starved of resources with the focus on Cube/HAL and new/broader STM32 part offerings.2018-02-26 3:21 PM
Dear Clive,
Our DfuSe utility is open and all sources code is provided since Years on the installed package using visual C++ Environment. So any one can customize it and modify .
Here above the main issue is coming from not accurate String descriptor on the page mapping fin our internal boot loader and can be re-worked at software level, we recommend using our new STM32Programmer that implement it and I can send you a patch for the old famous DFuSe .
Cheers,
STOne-32
2018-02-26 4:21 PM
The DfuSe 3.0.5 software hasn't been refreshed since 30-August-2015
Don't think it has support/updates for L4, L4+, F7 or H7
DFU Manager has 8-byte alignment issues on some parts due to the flash line size, and how the GNU Linker outputs generates images.
https://community.st.com/0D50X00009XkeovSAB
The All-In-One tools carries a lot of Java baggage
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.