2018-03-07 11:20 PM
Hello,
I'm developing an application based on STM32L475 device. So I need a timestamp on my application. I saw an RTC_timestamp example of NUCLEO-L476RG. So please anyone can tell how can I port this RTC_timestamp example of NUCLEO-L476RG to my STM32L475.
Best regards.
2018-03-08 1:24 AM
What, exactly, do you mean by 'timestamp' ?
If it just needs to be a number that increments at regular intervals, you could just use a simple timer - SysTick ?
how can I port this
same way that you'd port any other code:
L476RG
STM32L475 - if they are, job done!
If not, then update to match the
STM32L475
Or simply work from scratch - using the RTC can't be that hard, can it ... ?
2018-03-08 2:25 AM
thank you, Andrew Neil for the answer.
A timestamp is a record of time and date.
In my case, I get the sensor values continuously but I need a timestamp.So that I understand my sensors behaviour on a different day, time.
Right now I have my sensor values in this form.
But I need a date and time for every corresponding value. I hope now you understand my question.
2018-03-08 3:51 AM
Rai Ahmad wrote:
A timestamp is a record of time and date.
Not necessarily.
I need a timestamp.So that I understand my sensors behaviour on a different day, time.But you don't need to store the actual calendar date and wall-clock time to do that.
As noted, a simple count that increments at a known, regular interval would be sufficient.
In fact, if your sensor is being sampled
at a known, regular interval - then you don't need anything extra at all!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.