STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pull-up Resistor for NRST pin

Posted on March 28, 2018 at 03:10Hello,In the datasheet, it states that there is a pull-up resistor for the NRST pin but I was wondering if it is recommended to have a pull-up resistor for this pin.I have been using my customized development board w...

Justin K. by Associate II
  • 3478 Views
  • 2 replies
  • 0 kudos

ST32F1 CubeMX - I2C DMA - help needed

Posted on February 15, 2018 at 17:12Hi I'm trying to run I2C in DMA mode with LIS35 (accelerometer). I wrote simple code as below but each time when I try to run or debug it I'm getting back return ''LIS35_ERROR;'' which means that LIS35_I2C_Init(vo...

0690X00000604LDQAY.jpg 0690X00000604OGQAY.jpg

dereferencing type-punned pointer warning on bare project

Posted on March 28, 2018 at 20:53I decided to try out the new TrueStudio. Downloaded and installed it, and also updated STM32CubeMX to the latest, as well as all the latest firmware packages.I then created a new Cube project for TrueStudio using the...

STM32F051 - Flash not working with an external clock

Posted on March 26, 2018 at 15:16I have been trying to erase and store data in the flash without any success. As long as I am using the HSI clock to drive the SYSCLK, the flash works just fine. However, if I start using the external oscillator to dr...

Abi Nair by Associate
  • 2349 Views
  • 4 replies
  • 0 kudos

STM32F4 SDIO high speed write to sd card

Posted on April 07, 2016 at 14:15I've a following problem. I'm using STM32F427VG connected to microSD card via SDIO interface. I'm using ST driver, configured for 4-bit data access and DMA tranfer. I need to reach continuous write speed above 3000kb...

krestan by Associate II
  • 8728 Views
  • 13 replies
  • 0 kudos

Communication between STM32L4 and Blue NRG1

Posted on March 28, 2018 at 16:52Hello Can I configure the  STEVAL -IDB007V1 ( BLE NRG1 ) board as an expansion board with the STM32L476RGI must integer the driver bluetooth in STM32 L4 Nucleo but I could not configure the communication between the ...

Eya Eya by Associate
  • 691 Views
  • 0 replies
  • 0 kudos

We have managed to ''Brick'' an STM32F437ZGT.

Posted on March 28, 2018 at 11:34Hi, after running some software tests, we have locked the processor. In the past, I have managed to use a uLink2 debugger to unprotect the flash, and re-gain access.This time, the debugger won't even connect'Cannot a...

DMA counter resetting by itself

Posted on March 19, 2018 at 22:09Hello,Could someone tell me what I am doing wrong here?I would like to transmit on SPI (as slave) using DMA, and so have tied SPI transmit to a DMA channel, and set up an ISR to capture 'transmit completed' interrupt...

za kia by Associate II
  • 1443 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.