2018-03-26 6:16 AM
I have been trying to erase and store data in the flash without any success. As long as I am using the HSI clock to drive the SYSCLK, the flash works just fine. However, if I start using the external oscillator to drive the SYSCLK, any flash operation would freeze the MCU.
I am using an 8 MHz external oscillator. Initialization code that I use is provided below:
RCC_HSEConfig(RCC_HSE_ON);
RCC_PLLConfig(RCC_PLLSource_PREDIV1, RCC_PLLMul_6); // set the PLL Clock to 48 Mhz
RCC_PLLCmd(ENABLE);
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); // PLL selected as system clock source
RCC_HSI14Cmd(ENABLE);
RCC_HCLKConfig(RCC_SYSCLK_Div2); // HCLK selected as 24 MHz
RCC_PCLKConfig(RCC_HCLK_Div1); // PCLK selected as 24 MHz
RCC_ADCCLKConfig(RCC_ADCCLK_PCLK_Div2);
RCC_USARTCLKConfig(RCC_USART1CLK_SYSCLK);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);
RCC_LSICmd(ENABLE);
EDIT: Sorry. I am using an external 8 MHz oscillator (crystal), not an external clock.
#flash-storage #external-clock #stmf0512018-03-26 7:01 AM
Flash would have issues with wait-states at higher speed, and also issues if the power supply is marginal.
For an external 'source', ie TCXO, then you should use HSE BYPASS mode.
2018-03-27 6:28 PM
None of your code waits for anything to spin up properly
Check you have the flash set suitably
/* Enable Prefetch Buffer and set Flash Latency */
FLASH->ACR = FLASH_ACR_PRFTBE | FLASH_ACR_LATENCY;2018-03-28 7:57 AM
Thank you for your help. Flash latency is zero and I have not enabled the prefetch buffer as HCLK is 24 MHz. Should I implement a delay to initialize the clocks?
2018-03-28 9:23 AM
Try using some of the demo/example codes to see if they fail, and make a determination if it is a software issue or something specific about your board implementation.
Would suggest you clock the PLL at 24 MHz if that's how fast you want to run chip. You should follow directions in manuals with respect to waiting for resources to start properly, like ST's examples do.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.