STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Triple ADC regular simultaneous mode with DMA

Posted on April 03, 2018 at 08:57Hi,I am working on STM32F769NI-disc1 board. I am trying to get the triple ADC regular simultaneous mode to work with DMA. I have generated the code using the stmcubemx and with little understanding from the different...

LTDC & F746G-Discovery Timing

Posted on April 03, 2018 at 08:07I am wondering if the timings are set correctly in CubeMx for the LTCD Configuration for the F746G-Discovery board.  I find that if I run with the default settings in CubeMx for this board the display often is very n...

Using CubeMX to make a OTG FS VCP

Posted on April 03, 2018 at 04:33 I use CubeMX to make a OTG FS VCP, seems OK, data can transmit and receive, but there is a problem, PC software send a command to MCU, and I stop PC program, command keep received in MCU. I set a break point ...

how to setup for new MCU in I-CUBE-LRWAN

Posted on April 02, 2018 at 22:28HIIn I-CUBE-LRWAN it says that it is very easy to port to others mcu.Do anyone have a description how to setup a new MCU exsample STM32F303CCT6 ?1 .   If i make a cubemx project ..Which file to copy to the project an...

0690X00000604XrQAI.jpg
hjh by Associate III
  • 846 Views
  • 2 replies
  • 0 kudos

Resolved! Problem using DAC_OUT2 as COMP1 inverting input, STM32L4

Posted on March 12, 2018 at 16:31Hi,    I am having a problem using COMP1 on a STM32l496 chip.  I am doing a proof of concept on a Nucleo board.  I'm using a signal generator to put a 1KHz sine wave on the IN+ pin, and I'm using the DAC as the IN- s...

Resolved! STM32H743i & stmpe811

Posted on March 31, 2018 at 00:35I am trying to construct a CubeMX based version of the LwIP_HTTP_Server_Netconn_RTOS project in the repository.  I have used the board selector in CubeMx of the H743i-Eval and setup the options for the hardware to ma...

I2C startup

Posted on June 08, 2017 at 17:31 Edit: OK so just for the record, I guess, I replaced HAL_I2C_Master_Transmit_DMA() with HAL_I2C_Mem_Write(), which seems to be the appropriate command for what I'm doing, and that is working fine. One questi...

E P by Associate III
  • 1225 Views
  • 1 replies
  • 0 kudos

Can a STM32F407VGT6 LQFP-100 be replaced by a Stm32F7XX CPU?

Posted on April 01, 2018 at 17:04I have a PCB made for 100 pin F407. Is there a STM32F6 series CPU which works in that PCB? There seems to be a lot of 100 pin F6 CPUs. Is there something I should know, especially if I make a new PCB fit for both.#st...

LMI2 by Lead
  • 2509 Views
  • 5 replies
  • 0 kudos

STM32F030C6 trying to use LSE

Posted on April 02, 2018 at 11:26Hi, I have a STM32F0C6 board and I'm trying to use RTC function with LSE.It seems RTC is working correctly and I can check the waveform of LSE Clock from MCO pin.But when I check the waveform of OSC32_IN and OSC32_Ou...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.