STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F767ZI Pin Voltages are Too High

Posted on April 01, 2018 at 20:14The pin voltages are too high on my board. The (nominal) 5V pin measures 6.8V, and the 3v3 pin measures 4.7. The board appears to be running normally.I am powering the board via USB (CN1) JP1 is OFF. JP3 is set to U5...

STM32F103C8 as color video out source

Posted on April 02, 2018 at 10:53I want to use a STM32F103C8 as a standard NTSC color video out source. Arduino has a black and white video library that is compatible with most of thier boards. I figured the vastly more powerful STM32 could manage f...

VBUS PİN

Posted on March 30, 2018 at 16:31Hello everyone. I need to help immediately. I neet to disable VBUS pin on STM32F429. How can I do ? please help me 

Read Out Protection is Activated

Posted on March 31, 2018 at 14:21helloWorking on https://community.st.com/tags♯/?tags=stm32f4discovery%20stm32f4 Discovery Board, it was working fine but now whenever i erase or try to upload a code it say 'Read Protection is Activated', So how to r...

Resolved! Evaluation kit for STM32F733VE

Posted on April 02, 2018 at 05:55I am going to use STM32F733VE chip for AES encryption and USB feature. Can you recommend which evaluation kit and IDE should I use ? 

Hau Lam by Associate II
  • 1369 Views
  • 1 replies
  • 0 kudos

Help with selection of external memory.

Posted on March 29, 2018 at 11:25I am using DCMI peripheral to drive camera modules. At this point, I am able to obtain images with 320x240, 16 bits/pixel. I am working with a display connected via FSMC to the MCU and the display already provides en...

Running a 3.3V STM32F0 on 6.5V

Posted on March 31, 2018 at 19:35I'm using an STM32F0 in a high volume low power project running on a LIR2032 that can be charged via USB. The STM is specd at 2.4 - 3.6V, with 4.0V as the absolute maximum. When the battery is fully charged however t...

PB13 PiN of STM32F429 for CAN2

Posted on April 01, 2018 at 19:13Hello, First of all, I am sorry for my english. Then I am doing a application with CANBUS Protochol. so ı need to use PB13 pin of STM32F429. but when I use this pin, CAN2 is not work. When I look datasheet, this pin...

STM32F030 eeprom emulator

Posted on March 23, 2018 at 13:58HI I'm lookin for a eeprom emulator for a stm32F030 cpu,and if I go to : https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libr...

spa23 by Associate III
  • 1687 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.