STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 DISCOVERY UART + GPS

Posted on March 31, 2018 at 17:30Hey guys.I would like to receive NMEA lines from my GPS module with UART with STM32L476 DISCOVERY. Can you please help me how can I receive the full sentences? Because the length of the lines always differ, so with s...

Resolved! Core Clock speed

Posted on January 30, 2018 at 13:21hello is use stm32f30p4 and use 8000000 hse_value and use cmsis.i change SystemCoreClock in the system_stm32f0xx.c to 8000000 but my clock doesn't change and still work on 48MHZ.how can i fix it?SystemInit();System...

STM32F769i SBC manufacturers

Posted on April 03, 2018 at 09:15Hello,For a new project, we plan to develop the software on a STM32F769i-DISCO (discovery kit) with STM32Cube, but we need in a close future a true SBC board.Who are the manufacturers of true SBC cards with STM32F769...

STM32F733VE connect to the eMMC

Posted on April 03, 2018 at 12:24I'm going to use STM32F733VE to connect to the eMMC. Is it possible ?If it possible , which port should i use , does it use the sane SD/MMC port ? And how to i approach this solution ? 

Hau Lam by Associate II
  • 544 Views
  • 0 replies
  • 0 kudos

LL_code does not use SystemCoreClockUpdate?

Posted on April 03, 2018 at 11:15Using:Truestudio for STM32 v9.0.0.0STM32CubeMX v4.25.0STM32F100C8LL_drivers onlyIn stm32f1xx_ll_utils.c the SystemCoreClock variable is set directly:void LL_SetSystemCoreClock(uint32_t HCLKFrequency) {    SystemCoreC...

Willunen by Associate III
  • 846 Views
  • 0 replies
  • 0 kudos

stm32, 485 bus

Posted on April 03, 2018 at 08:25Hi. I'm testing a new board with a STM32F091rctx micro, where the 485 bus is bring up using these pinouts:PB5 (Enable)PD2 (Rx)PC12 (Tx)Is the Enable signal moved by the Hal libraries or have I to move it?Using an osc...

stm32 RCC

Posted on April 03, 2018 at 08:43I want to ask about RCC registers.  Can I change the divider values PLLMUL and HPRE in Runtime?The program code is then executed to reduce the frequency (decrease in consumption), then increasing the frequency and ex...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.