STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-L4R5ZI Debug issue.

Posted on April 06, 2018 at 13:04Hi Team,I have issue in debugging NUCLEO-L4R5ZI, i m facing with following error, for the IOToggle code.Please let me know what i need to change in the below script. to fix the issue to proceed in debug.IDE: Atollic ...

0690X0000060ASYQA2.png

RM0394 reference manual Errors

Posted on April 06, 2018 at 23:54For the next update to RM0394 ('Reference Manual - STM32L43xxx STM32L44xxx STM32L45xxx STM32L46xxxadvanced ARM®-based 32-bit MCUs'):=========On page 74, in the table showing page locations in memory, it shows page 2...

STM32F0 deep sleep with TIM1 as time-base source

Posted on April 09, 2018 at 10:49Hi,I having a problem to get in sleep mode when using TIM1 as time-base source instead sysTick.When using sysTick I'm able to enter sleep mode with no problem.I wish to use TIM1 as time-base source to be able to use ...

Ariel G by Associate II
  • 800 Views
  • 0 replies
  • 0 kudos

key derivation in chip stm32f733ze

Posted on April 09, 2018 at 06:20I'm trying to use AES function in chip stm32f733ze .Can I know whether this chip can support Key Derivation function or not ?Because from the Reference Manual  RM0431 it said that the chip only support 4 modes :' The...

Hau Lam by Associate II
  • 765 Views
  • 0 replies
  • 0 kudos

Request Idea for programmer STM32L4

Posted on April 09, 2018 at 05:43WE have new project for program STM32L486,With command line.One target and one programmer(ST-Link V2).Every think OK.But,now we update to 6 target and 6 programmer,. We have only one PC control.Who have ever do befor...

0690X00000602VoQAI.bmp

RDP Setting, HAL_FLASH_OB_Launch(), holding

Posted on April 09, 2018 at 04:17Hi.I am going to set the RDP-Level 1 programmatically.Here is the test code:Here it stops at the HAL_FLASH_OB_Launch () function.The Reset button does not work in this state.The USB connection will work only if you r...

stm32 2G module

Posted on April 08, 2018 at 04:03HI   I use stm32f107?now I want to communicate with a 2G gprs module by usb?How I do it ?#stm-32 #stm-32lo #stm-32f107 #stm-mcu

fan li by Associate
  • 1349 Views
  • 2 replies
  • 0 kudos

STM32f302cc SPI code assistance needed

Posted on March 25, 2018 at 22:51Hi,I have recently move from the STM32f101 to the stm32f302, I am using atollic IDE and the Hal library for the initial configuration of the peripherals.  I use register level setup for a lower overhead. having said ...

conrad c by Associate II
  • 3696 Views
  • 7 replies
  • 0 kudos

stm32R7VI widebus

Posted on March 24, 2018 at 10:29I met an interesting problem. When I tried to configure this IO with SD widebus config (4bit) with hal libraries I always failed with initialization because pin 1 of SD card is on logic 0.The solution was firstly let...

semler by Associate II
  • 3068 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.