cancel
Showing results for 
Search instead for 
Did you mean: 

key derivation in chip stm32f733ze

Hau Lam
Associate II
Posted on April 09, 2018 at 06:20

I'm trying to use AES function in chip stm32f733ze .

Can I know whether this chip can support Key Derivation function or not ?

Because from the Reference Manual  RM0431 it said that the chip only support 4 modes :

' The AES features the following modes of operation:

• Mode 1:

Plaintext encryption using a key stored in the AES_KEYRx registers

• Mode 2:

ECB or CBC decryption key preparation. It must be used prior to selecting Mode 3 with

ECB or CBC chaining modes. The key prepared for decryption is stored automatically

in the AES_KEYRx registers. Now the AES peripheral is ready to switch to Mode 3 for

executing data decryption.

• Mode 3:

Ciphertext decryption using a key stored in the AES_KEYRx registers. When ECB and

CBC chaining modes are selected, the key must be prepared beforehand, through

Mode 2.

• Mode 4:

ECB or CBC ciphertext single decryption using the '

So i have a little bit confuse .Could you support me this issue ?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.