2018-04-06 2:54 PM
For the next update to RM0394 ('Reference Manual - STM32L43xxx STM32L44xxx STM32L45xxx STM32L46xxx
advanced ARM®-based 32-bit MCUs'):=========
On page 74, in the table showing page locations in memory, it shows page 255 being at location:
0x087F F800 - 0x087F FFFF
That should be:
0x0807 F800 - 0x0807 FFFF
==========
At the top of page 81, in the steps for 'Mass Erase' (title is on previous page), step 4 is:
4. Set the STRT bit in the FLACH_CR register.
it should be:
4. Set the STRT bit in the FLASH_CR register.
==========
On page 81, in the steps involved in 'Standard Programming', step 7 is:
7. Clear the PG bit in the FLASH_SR register if there no more programming request
anymore.It should be:
7. Clear the PG bit in the FLASH_CR register if there no more programming request
anymore.=========
On page 82, in the steps for Fast Programming, step 8 is:
8. Clear the FSTPG bit in the FLASH_SR register if there no more programming request
anymore.It should be:
8. Clear the FSTPG bit in the FLASH_CR register if there no more programming request
anymore.2018-04-08 4:26 PM
Found another one: On page 103
Bit 16 START: Start
should be :
Bit 16 STRT: Start
It is spelled correctly in the description that follows, and in the chart on the previous page. But not here.
2018-04-09 1:53 AM
Hello
Jones.Dave.002
,Thank you for all reported typos.
This is passed internally to the appropriate team for correction in the coming releases.
Best Regards,
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.