STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L073RZ microsecond Delay

Posted on April 23, 2018 at 15:23Hello ,I am using STM32L073RZ MCU for my project to generate one microsecond delay for one wire protocol but i am unable to get,Can anyone help me to get microsecond delay and how to set prescalar value and clock per...

Nagesh A by Associate
  • 993 Views
  • 1 replies
  • 0 kudos

STemWin screen rotate

Posted on June 27, 2017 at 14:04Hello everyone!I have a 32f429i_disco_MB1075, I have succesfully ran an freeRTOS os with STemWin. Everything is working fine, but I have to rotate the screen. The GUI_Rotate function doesn't seem to work and I believe...

SimonP by Associate II
  • 2069 Views
  • 3 replies
  • 0 kudos

[Bug Report] CubeMX generated I2C init has flaw

Posted on April 17, 2018 at 00:13I don't know if there's a non-forum place to send CubeMX bug reports, so I'm putting it here.I found this when generating a CubeMX project for the STM32L452 with the I2C ports created using LL code..In the I2C initia...

clk frequency output problem

Posted on April 13, 2018 at 11:13 Hi, I use the STM32CubeMX to send data using UART, but I have a clock frequency problem, I configured the clk as shown on the picture below logically, I should obtain 80MHZ as an outpout frequency, but w...

0690X0000060AaOQAU.png 0690X00000604aRQAQ.jpg 0690X00000604a2QAA.jpg

CubeMX clock configuration fails for L4R5ZI chips

Posted on April 10, 2018 at 15:32Why does the STM32CubeMX tool in my Nucleo-L4R5ZI-based project disallow HCLK frequencies below 15 MHz? According to the datasheet frequencies as low as 100 kHz should be possible.When writing this: The current eclip...

Question about interrupt debugging in IAR

Posted on April 23, 2018 at 12:01I'm using STM32F103 and I was doing the following procedures:1) Break the execution using IAR debug function2) Generate a software EXTI by wring '1' to the EXTI->SWIER93) Observe the EXTI->PR9 become '1' which is cor...

Kefei Yao by Associate III
  • 1002 Views
  • 0 replies
  • 0 kudos

Write problems on a SRAM with the STM32H743ZIT6

Posted on April 20, 2018 at 14:19GreetingsI have the following problem on the micro STM32H743ZIT6:1) during access to the external write bus, on an SRAM, with only 16 bit bus, occurs when I execute the instruction* ((uint16_t *) 0x60000000) = (uint1...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.