STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

i need to connect two stm32 udp with a switch to pc

Posted on April 26, 2018 at 09:33 hello when i connect two stm32 one ip 1.1.88 port 88 the other one is 1.1.70 port 70 to a with switch device using udp to a remote pc ethernet ip 1.1.89 , if one send data the other stm cannot send ???? separatly t...

How to use the STM32 Ecosystem Software

Posted on April 30, 2018 at 15:58Hi Everyone!   Greetings from Argentina!   Please, Could you tell me how to use the STM32 Ecosystem Software, to create the necessary files for a Board Support Package to be able to develop in Keil uVision MDK.   The...

STM32F746 + Lwip, MCU load due to broadcast ???

Posted on May 02, 2018 at 11:03Due to the wrong network configuration, It is assumed that broadcast packet looping has occurred.STM32 MCU continuously receives broadcast packets.As a result, the MCU load increases.Tested on the STM32F746G-DISCOVERY ...

SWV issue getting the Garbage Values

Posted on May 01, 2018 at 14:09I was trying to get the debug statements on the SWV on Nucleo64 STM32F302R8. I tried the tutorial ''https://www.youtube.com/watch?v=BwgPV3uKuzY'' by Atollic Tools but had no success it prints out Garbage Values. Is the...

0690X00000604A1QAI.jpg 0690X00000604eEQAQ.jpg 0690X00000604bzQAA.jpg 0690X00000604fRQAQ.jpg

STM32F4 RTC problem

Posted on May 02, 2018 at 14:51Hello,I have a problem. I use a STM32F427 with Keil RTX.If I start my Programm without a backup battery my Programm runs into a rtos error (stack Overflow) if I want to set the date/time, but at this time the os isn't ...

Mearsure CPU Load

Posted on May 02, 2018 at 14:42Good afternoon everybodyI am a beginner, and I have a question about CPU load.How can I measure CPU load value from STM32F07 kit ?

Resolved! TIMER 3 Interrupt

Posted on April 25, 2018 at 13:01Hi all,This is a question regarding STM32F0 TIM3.I have written this code in keil compiler/***** main.c*****/&sharpinclude<stm32f0xx.h>&sharpinclude<stm32f030x8.h>void GPIO_Init(void);  void TIM3_Init(void);int main(...

sanju by Senior
  • 6416 Views
  • 7 replies
  • 0 kudos

Problem reading MAX17205 Fuel Gauge over I2C

Posted on April 30, 2018 at 10:52Hi,I have a MAX17205 Fuel Gauge connected to an STM32373C-EVAL board over I2C. I'm trying to read the DEVNAME register on the MAX17205 as a communication test but am getting a NACK error. I've checked the I2C signals...

MX_RTC_Init STM32CubeMX 4.24 error

Posted on January 31, 2018 at 13:44Hello! I've found a bug in RTC adjustment, when I used STM32CubeMX 4.24 for STM32L0.MX_RTC_Init does not activate RTC because of HAL_RTCEx_BKUPRead/HAL_RTCEx_BKUPWrite 'guard'. For example, 4.23 version did not wra...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.