2018-03-20 7:18 AM
On STM32L476RETx
void SystemClock_Config(void){
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct; RCC_PeriphCLKInitTypeDef PeriphClkInit;// ...
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|
RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
RCC_OscInitStruct.LSEState = RCC_LSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.MSIState = RCC_MSI_ON;
RCC_OscInitStruct.MSICalibrationValue = 0;
RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_11;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
// NO RCC_OscInitStruct.PLL.PLLM initialization !
// should be = 1 but is = 0 by default so it triggers assert_failed and _Error_Handler
RCC_OscInitStruct.PLL.PLLN = 10;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
Thanks
Romain
Solved! Go to Solution.
2018-05-10 9:45 AM
Hi
Lamothe.Romain
,CubeMX version 4.1
(in which thisissue is resolved) isavailable now on ST Website.
Regards,
Houda
2018-03-22 9:18 AM
Approved, I have the same issue (CubeMX 4.25.0).
2018-03-22 5:19 PM
And if you dont use full assert, and build it, your system core clock speed starts at half speed, then goes down each time you hit the reset button. Got it as low as 11mhz, from 40. When it should have been 80.
2018-03-22 5:42 PM
Would also strongly recommend the use of the RCC_OscInitTypeDef RCC_OscInitStruct = {0}; form to ensure that the auto/local variable actually gets initialized to something predictable, normal behaviour exposes random stack content.
2018-04-03 11:19 AM
This issue is a CubeMX problem.
4.24 produces the correct RCC PLLM
4.25 does not.
I posted something to tech support a while back on a previous version, maybe 4.22, that does not produce RCC PLLM in the main.c initialization when you are using the PLL as a system clock. I use MSI to PLL for my system clock.
4.23 produces RCC PLLM and I think 4.21.1 does as well.
I don't advise using this as a work around but rather a test. IF you go into the .ioc file and change
MxDb.Version=DB.4.0.250
to
MxDb.Version=DB.4.0.240
then the PLLM initialization will come back.
I generated 3 projects using the same source for import to verify that PLLM is generated using 4.24 and 4.23.
According to the CubeMX change log there were a lot of changes when they went from 4.23 to 4.24 so I'm hesitant to use 4.24 and 4.25 doesn't work so I'm still using MXCube 4.23 until they get the PLLM generation figured out.
Roman
2018-04-04 6:47 AM
Hello,
You are right, PLLM parameter
is no more generate for STM32L4 in the CubeMX
version 4.25
.T
hisCubeMX bug passed internally to CubeMx team -again- for fix as it seems to be a regression issue after being fixed in version 4.23 and in version 4.25 for L4+ (asmentioned in the Release note of STM32CubeMX
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Frelease_note%2Fb2%2F02%2F4b%2Fe3%2F81%2F32%2F49%2Fc4%2FDM001076pdf%2Ffiles%2FDM001076pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.DM001076pdf
).Sorry for such inconvenience.
Best Regards,
Imen
2018-04-12 1:58 AM
Hello Motla,
Thanks for your feedback
The issue will be fixed next CubeMX release.
Please feel free to contact me for further details.
Best regards,
Houda
2018-04-12 7:45 AM
Hello Houda,
Are there any other STM32L4xx issues if I were to use CubeMX 4.25 besides it omitting the PLLM setting?
Roman
2018-05-10 9:45 AM
Hi
Lamothe.Romain
,CubeMX version 4.1
(in which thisissue is resolved) isavailable now on ST Website.
Regards,
Houda
2018-05-10 12:20 PM
Wonderful,
Thanks,
Roman Marjamaa
Marjamaa Engineering Inc.
395 Co Rd 110 N
Mound, MN 55364
Direct: (612) 999-8263
Mobile: (612) 345-1492
Fax: (855) 627-5364
www.marjamaaengineering.com<http://www.marjamaaengineering.com/>;
All information contained in this email is to be treated as “confidential� or “proprietary� and shall not be shared
outside the terms of the Agreement between Marjamaa Engineering Inc. and the Recipients of this email.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.