STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L151C8T6 RTC wakeup not counting

Posted on June 08, 2018 at 15:25Hello,I try to have a periodic wakeup of my chip.I read the RTC documentation, and I tried to setup the RTC periodic wakeup unit.I managed to get a periodic interruption but I don't understand why the counter is not c...

HAL I2C Slave Sequential Receive pulling SDA pulled low

Posted on June 08, 2018 at 15:04 Hi, I've got a weird problem with I'd like some advice on. I've configured an STM32F334 as a I2C Slave, and am using Sequential IT driven operation with variable length packets (e.g. first byte received is length ...

0690X0000060L1SQAU.png
sasha by Associate III
  • 1733 Views
  • 0 replies
  • 1 kudos

SWCLK AND SWDIO ?

Posted on June 07, 2018 at 21:58Hi,i am beginner in stm32I configured SWCLK AND SWDIO for Serial Debugging.Can I Change SWCLK and SWDIO as input and output at runtime?If Change the MCU is RESET or Not?

The problem of STiD135 ts

Posted on June 08, 2018 at 13:26hi, I am a beginner of stid135, I had a problem when I tried to configure stid135 to output TS. I used PRBS11 as the data source of a dvb modem to modulate a dvb-s signal, then to use development board STiD135 NIM_B22...

Trouble with one VDD pin of STM32F103

Posted on June 08, 2018 at 09:15I use STM32F103CBT6 for my project. This is something trouble this time. One of VDD pins of MCU is broken and not have connection to pcb. Another three pins are fine. Would MCU work fine if i not resoldering it and wo...

STM32 compatibility with PIC18

Posted on June 07, 2018 at 16:26Hello everyone,I am currently working on a traveler counting system that is based on a PIC18 and I would like for network link reasons to make a serial link (RS232), in fact, a new standard of transport, to put in dis...

STM32L031 multichannel ADC

Posted on June 08, 2018 at 11:47HiI'm trying to read ADC 6 channel but I got very strange result 60 or 4095 not the right one...Any help are welcome  what I'm doing wrong.  I need without DMA if possible without?main initstatic void MX_ADC_Init(void...

Andy b1 by Associate II
  • 817 Views
  • 0 replies
  • 0 kudos

configuration of ''USART'' without CubeMX

Posted on June 05, 2018 at 14:48 Hello, i use the stm nucleo 64 board and the stm/eclipse environment and i want to send string with usart1. Furthermore, i don't want to use cubemx and cmsis. Because it makes the code very unreadable... and I'...

Toby _ by Associate II
  • 5614 Views
  • 16 replies
  • 0 kudos

ADC Glitch

Posted on June 08, 2018 at 02:22Hello everyone,We have a MCU STM32F427. There are 5 ADC channels. During our testing, we found there is ADC glitch, see attached picture. There are 2 significant drop in ADC.Do you know the reason that cause the ADC g...

Pilot B by Associate II
  • 2349 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.