2018-06-08 6:25 AM
Hello,
I try to have a periodic wakeup of my chip.
I read the RTC documentation, and I tried to setup the RTC periodic wakeup unit.
I managed to get a periodic interruption but I don't understand why the counter is not changing.
void RTC_WKUP_IRQHandler(void)
{ printf('IT RTC %u\n', RTC_GetWakeUpCounter()); if(RTC_GetITStatus(RTC_IT_WUT) != RESET) { RTC_ClearITPendingBit(RTC_IT_WUT); EXTI_ClearITPendingBit(EXTI_Line20); } }I always get 'IT RTC 65535', everytime the handler is called (once every second in my case).
Here is my initiliazing code :
// RTC periodic wakeup
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR, ENABLE); PWR_RTCAccessCmd(ENABLE); RCC_RTCResetCmd(ENABLE); RCC_RTCResetCmd(DISABLE); //MSG('wait HSE'); RCC_HSEConfig(RCC_HSE_ON); while (RCC_GetFlagStatus(RCC_FLAG_HSERDY) == RESET) {} RCC_RTCCLKConfig(RCC_RTCCLKSource_HSE_Div8); RCC_RTCCLKCmd(ENABLE); //MSG('wait synchro'); RTC_WaitForSynchro(); EXTI_InitTypeDef EXTI_InitStructure; EXTI_ClearITPendingBit(EXTI_Line20); EXTI_InitStructure.EXTI_Line = EXTI_Line20; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Rising; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_Init(&EXTI_InitStructure); NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = RTC_WKUP_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); RTC_WakeUpClockConfig(RTC_WakeUpClock_RTCCLK_Div16); RTC_SetWakeUpCounter(0xFFFF); RTC_ITConfig(RTC_IT_WUT, ENABLE);RTC_WakeUpCmd(ENABLE);
You can see the 0xFFFF used to initialize the counter (only once).
I tried to change it : I saw the new value in the interrupt printf, and the call to the interrupt changed also.
So the value is used to know when to trigger the interrupt, even if the value doesn't change
What am I missing so that the RTC wakeup counter correctly decrements?
Or am I missing the point, and the value does not decrement at all?
#stm32l1-rtc #stm32-rtc #rtcWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.