STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Please teach me about FSMC in STM32 MCU

Please teach me about FSMC in STM32 MCU. When the CPU communicates with external MRAM, can FSMC be used?   <MRAM specifications> Interface Type:Parallel Data Bus Width:16 bit

Junki by Associate
  • 1629 Views
  • 3 replies
  • 0 kudos

Resolved! STM32H7 - MPU Configuration

Hi All, I was testing my new STM32H746XIH6 board and met the post below by @GSpre.1 during a search about SDRAM  performance. GSpre.1 - Performance characteristics of SDRAM on STM32F7508-DISCO board I don't have a lot of time to read MPU documentatio...

Resolved! FDCAN Receive FIFO0 FIFO1 STM32H5

Hi,this is my MCU code: STM32H563VGT6. I'm working to a porting from Texas to ST.I need to efficently use the two Rx FIFO (3 messages depth) of the FDCAN module. In Texas I had 32 mailbox divided into transmission and reception.Each FIFO has four buf...

DAUSILI by Associate III
  • 1743 Views
  • 2 replies
  • 3 kudos

Resolved! Most basic setup for SWD to work?

Hello, i need help with na stm32l031k6, I want to just start the processor and read it with an st-link v2, I have connected BOOT0 to GND(i haven't added a 10k resistor, but that shouldn't be the problem ), NRST with pull-up 1k to VDD, VDDA and VDD ar...

LubO_o by Associate
  • 2324 Views
  • 3 replies
  • 5 kudos

Resolved! stm32F429BI + LCD does not switch-on the display

I am starting some test with this modulehttps://it.aliexpress.com/item/1005002482177244.htmlwith 7” lcdI have found only one example that run but with TouchgfxI have got the same ioc from this example to generate a new code and insert the functions t...

Ciuffoly by Senior
  • 13934 Views
  • 46 replies
  • 1 kudos

Resolved! Periodic PC sample packets via DWT

I am trying to persuade an stm32F412 to provide Periodic PC sample packets.Reference manual RM0402 implies it is doable (Configure DWT as a PC sampler)The "Cortex-M4 Technical Reference Manual r0p0" says "You can configure the DWT to generate PC samp...

Scopi by Associate II
  • 1301 Views
  • 1 replies
  • 0 kudos

Resolved! Custom board with STM32f446rRE: JTAG TDI not successful

Hello everyone,I am developing a custom PCB and am having a problem while trying to flash the chip.Before delving further, I need to say that I have made a mistake with routing the JTAG traces to 10pin JTAG connector and may have burnt the chip. I tr...

jtag_circumvent.jpg sys.png pins.png 70nKA_0-1742223736249.png
70nKA by Associate II
  • 1244 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.