STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory management fault on OTP reading

I have ported an application to STM32H563ZI which uses the OTP area to store a key. MPU is configured. Reading the UID is possible. void Mpu::Config(void) { MPU_Attributes_InitTypeDef attr{}; MPU_Region_InitTypeDef region{}; /* Disable...

Donnie by Associate
  • 1975 Views
  • 3 replies
  • 0 kudos

STM32G484 usage of pins OSC32_IN/OUT as GPIO

Hey all :)We have designed a board with the STM32G484VEH6 and need to use OSC32_IN/OUT (PC14/15) as GPIO pins. We use PC15 as an interrupt pin for a connected SPI device and PC14 as GPIO output.Unfortunately neither the interrupt nor the GPIO output ...

ADC readings

Hello,    I have a problem witht he ADC readings and the timing of reading of the ADC channels.   I am currently using an STM32 U545, both ADCs (1 & 4) configured to read voltage values comming from different sensors that i have on my pcb. The ADC is...

Marc3_0-1742807506325.png
Marc3 by Associate III
  • 2508 Views
  • 5 replies
  • 0 kudos

Power consumption of STM32L412XX

Hi, I am doing a comparison between the STM32L432 and the STM32L412. However, I observed a discrepancy in the STM32L412 power values under Table 4. STM32L412xx modes overview, LPRun and LPSleep are showing the same value. Is this correct?  

akhilfrancis_0-1742620945851.png

stm32U545RE_Q RTC wake up from standby mode

I am using an stm32U545RE_Q and want to put my device into standby mode and then periodically wake it up (every 10s). but it doesn't work   Am I missing something or how am I supposed to continue from here?   /* USER CODE BEGIN Header */ /** *****...

스크린샷 2025-03-24 144302.png 스크린샷 2025-03-24 144307.png
dlagyals by Associate II
  • 1042 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H563 VDDA rising and falling control timig

I'm thinking to control for VDDA on the STM32H563.I'm considering by the red line in the diagram below, but are there any problems?I'm considering when VDDX independent from VDD, can be rising and falling VDDA.Please advise for me.Best regard.     

tomy_2-1742551132059.png
tomy by Associate II
  • 2035 Views
  • 5 replies
  • 0 kudos

Low power STOP1 mode current consumption high

Hello,I am using STM32G4 to develop a project where I am running FreeRTOS.Recently I was working on debugging the issues for low power mode.I can confirm all the peripherals clocks are disabled before entering the STOP1 mode, but the power consumptio...

Long Timer interrupt routine

I am using STM32F100. I wrote a very long code for my timer interrupt. If the processing time of this code exceeds the interrupt duration, can a pin I SET be RESET?

XooM by Senior
  • 3071 Views
  • 6 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.