STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CAN FIFO0 and FIFO1 stm32f429

Posted on June 14, 2018 at 08:37Hello,Could you describe difference in use FIFO0 and FIFO1 for CAN1 and CAN2 in stm32f4 mcu? For example if I configure CAN2 for receive in FIFO0 and configurate filters 14 all work success, but if I try use FIFO1 wit...

kruft by Associate III
  • 11627 Views
  • 16 replies
  • 0 kudos

Wrong flash latency from CubeMX with STM32F302CC?

Posted on May 19, 2018 at 19:51My program crashes with the following error in TrueStudio:''Program received signal SIGTRAP, Trace/breakpoint trap.0xfffffffe in ?? ()''The fault occurs in line 692 of stm32f3xx_hal_rcc.c:__HAL_RCC_SYSCLK_CONFIG(RCC_Cl...

0690X0000060KnzQAE.png

STM32L476 lowest sleep current with RAM retention

Posted on June 13, 2018 at 11:18Hello,Which is the mode which permits the lowest current with RAM retention for variables?In this mode which is the current consumption for the STM32L476?Best regardsMich

Mich1 by Associate III
  • 2465 Views
  • 4 replies
  • 0 kudos

STM32L4 usb_mic clock config

Posted on June 15, 2018 at 11:45hello,I'm trying to implement a USB microphone using STM32L4 discovery board.I have started with the USB device example and now trying to add the microphone.The library have given us the stm32l476g_discovery_audio.cwi...

SPI1_TRANSIT problem

Posted on June 15, 2018 at 10:33Hello, I realized a few weeks ago a code that works on a nucleo card with the following RF module X-NUCLEO-IDS01A4, this one contains SPSGRF-915. I have now adapted this program for a prototype containing the SPSGRF-8...

0690X0000060LHjQAM.png

stm32f746 disco USB CDC

Posted on June 12, 2018 at 10:07Hello,I try run a USB CDC on my eval board using USB FS. I generate from cubeMX a code with CDC, set a clocks (HCLK sets on 216MHz and 120MHz but USB clk on 48MHz) A clear code from cubeMx should cause that windows fi...

gd_jagi by Associate
  • 1403 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.