STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About SWD signals

Posted on June 14, 2018 at 16:00Hello, please tell me, what is the minimum number of signals required for the SWD interface: SWDIO, SWCLK? NRST is also required or possible without it?

v_tamakov by Associate II
  • 2626 Views
  • 4 replies
  • 0 kudos

SPTM34 Eval baord measure current

Posted on June 15, 2018 at 17:43Hey guys, I am using a STPM34 Evaluation board with a  STEVAL-IPE023V1 USB interface to measure a current from a simple circuit through SPI interface. for some reason I always read 0 for the current for C1 and 4.6189 ...

Ling Wu by Associate
  • 1346 Views
  • 0 replies
  • 0 kudos

Resolved! the HAL has BUG of CAN drive on STM32F1?

Posted on June 14, 2018 at 19:23Stm32F103 HAL_CAN_Transmit(&hcan,10) not working, always return HAL_TIMEOUT and HAL_ERROR, but when i use STD_Lib everything is good. So i think if the HAL has BUG of CAN on STM32F1?Hello,I'm trying to set up CAN on m...

Wei RP by Associate II
  • 1747 Views
  • 3 replies
  • 0 kudos

SPI_DMA Slave Receive only after reset

Posted on June 15, 2018 at 07:53Hi stI try to recieve spi dma slave by stm32f746 as slave i send two bytes for test from master raspberry when reset mcu it receive ok  when i repeat request it receive nothing and rx buffer not changedi tried checkin...

egywell by Associate II
  • 1404 Views
  • 2 replies
  • 0 kudos

n-Pulse generation : REP_CNT register

Posted on September 13, 2017 at 23:53I am using https://community.st.com/0D50X00009XkdsSSAR method to drive a servo-like motor interface. In the system, if E-Stop is pressed, I'lI have stop the motor immediately. Is there a way to find out the numbe...

Neo M by Associate II
  • 1258 Views
  • 3 replies
  • 0 kudos

STMStudio Issue - no more data stream

Posted on June 14, 2018 at 22:58Hello!I used STMStudio on the NUCLEO-F303RE for plotting signals and it worked fine. Now I built my own PCB with an STM32F303RC, broke off the debug-part of the NUCLEO board and startet debugging with the SWD connecto...

X-Nucleo-IDB05A jumper issue

Posted on June 15, 2018 at 13:28Hi !We are working with X-nucleo-IDB05A1, we had some disconnection issue without reason. and we figure out that there is HCI_DISCONNECTION_EVT generated each time. The reason is connection timout ,which can be genera...

Can't make I2C START condition on stm32l100

Posted on June 15, 2018 at 13:26I'm using stm32l100C6-A to communicate with gas gauge by I2C. My code tries to start I2C transfer, like this:I2C_GenerateSTART( i2c_periph, ENABLE );and sometimes it works, transfer is completed, all is well. But some...

0690X0000060BgqQAE.png
amomum by Associate III
  • 971 Views
  • 0 replies
  • 0 kudos

Resolved! New chips with U suffix.

Posted on August 10, 2016 at 09:39I am used to chips being marked for example ''STM32F405VGT6''. However, from several people I hear that now chips marked with an additional ''U'' at the end are showing up. Date code 1613 or something like that. One...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.