STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TrueStudio update error

Posted on June 15, 2018 at 04:35Hi All, Would you please take a look at following error of TrueStudio being happened during 'Check update' ?================Cannot complete the install because of a conflicting dependency. Software being installed: C/...

关于EVCR与EVENTOUT

Posted on June 15, 2018 at 04:31我在使用STM32F103,我在资料上看到�?�以�?置AFIO_EVCR,选择�?个IO作为检测到端�?�上的事件�?�的脉冲输出。�?�设,我现在�?置了AFIO->EVCR寄存器,选择了PB0作为EVENTOUT输出�?�;根�?�GPIO�?�的外部中断/事件框图我选择PA1作为外部事件检测�?�,我�?�时�?置了EXTI_EMR,EXTI_FTSR寄存器,使得PA1是带上拉的输入�?�,开�?�事件请求,下�?沿触�?...

0690X0000060LH0QAM.png 0690X0000060LHFQA2.png

ADC calibration on STM32F207

Posted on June 13, 2018 at 03:26Hi all,I am searching for STM32F207 ADC calibration and not very clear about if the MCUs of this series do ADCself-calibration.I have also checked the data sheet and reference manual but could not find a description o...

Recovering information after software reset

Posted on June 14, 2018 at 16:39My program executes a software reset under certain conditions using  'NVIC_SystemReset();'Before executing the reset I need to set a variable that will still be accessible after the reset so the program can understand...

Resolved! Reset timer counter on Input Capture

Posted on June 14, 2018 at 01:13I have configured an timer IC channel and it is working ok however the timer counter isn't reset when I read the captured value: void HAL_TIM_IC_CaptureCallback(TIM_HandleTypeDef *htim){if (htim == &htim2)    {       ...

ee06091 by Associate III
  • 5433 Views
  • 5 replies
  • 1 kudos

reset on nucleo -f401RE with even very simple main loop

Posted on May 24, 2018 at 22:20Dear Sir/Madam:I am using nucleo -f401RE with STM32 . I found the program keeps reset even with almost empty main loopthere is no way to do seftreset from the codes. only settings for hardware are system clock and some...

Resolved! Broken Forum Login

Posted on May 18, 2016 at 20:54The forum has been a mess the last few days. Only ''sign-on to forum'' seems to work, entering username/password on message replies just results in all sorts of error screens/pages. TCP connect or somesuch. #worst-f...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.