STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L072 Adc Vref source

Posted on June 16, 2018 at 20:16Hi,I'm a little bit confused about adc and vref.From reference manualThe internal voltage reference (VREFINT) provides a stable (bandgap) voltage output for theADC and Comparators. VREFINT is internally connected to t...

sukoy27k by Associate II
  • 2206 Views
  • 2 replies
  • 0 kudos

Working with TIM Output Compare

Posted on June 16, 2018 at 23:08I try to generate pulses for the stepping motor at the Output Compare output.The time between their leading fronts varies (acceleration / deceleration).The control of delays based on the well-known principle: free run...

0690X00000604hhQAA.jpg

STM32L4 QSPI flash memory mapped

Posted on June 16, 2018 at 14:32 Hello there, In the device I am developing on STM32L452 I foresee running out of flash memory, as the application code is getting bigger. The maximum flash amount for this chip is 512 KB (which I use). I thought I...

STM32 RTC milliseconds setting

Posted on June 07, 2018 at 03:50Hello,I'm using the STM32 H753 Evaluation board, and trying to set the milliseconds by using HAL_RTC_SetTime function.However, the HAL_RTC_SetTime function does not change the milliseconds(subseconds) value.I've read ...

STM32F4DISCOVERY Register Level Programming

Posted on June 09, 2018 at 04:32Hi Everyone,    I am new to stm32f4 series. I have done GPIO example using libraries. But i wanted to do register level programming. I have tried it but i could not get output for this. Can anyone help me out?&sharpin...

Yadav by Associate II
  • 5016 Views
  • 23 replies
  • 0 kudos

Resolved! STM32F407 ADC LOWER LEVEL PROGRAMMING ISSUE

Posted on June 12, 2018 at 06:37Hi Everyone,       I m interested in doing lower level programming. Now i currently working with stm32f407 board. I have successfully got the output for GPIO. Now i am started working on ADC interface. But i couldnt g...

Yadav by Associate II
  • 4824 Views
  • 9 replies
  • 0 kudos

Resolved! SD read/write with DMA mode working only in debug mode

Posted on May 29, 2018 at 13:55Hi All,I am working on STM32F413 Disco kit and trying to read/write into SD card using DMA mode.My requirement is -   i have to call single function which will read/write into SD card in 1ms timer callback function.It ...

can't escape while loop in SystemClock_Config();

Posted on June 14, 2018 at 09:35So i noticed something interesting. When setting up a project with cube or looking at a ST example for USB host the Config for system clock is like this.RCC_OscInitTypeDef RCC_OscInitStruct;RCC_ClkInitTypeDef RCC_ClkI...

td by Associate II
  • 2987 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.