2018-06-14 10:53 PM
Hi st
I try to recieve spi dma slave by stm32f746 as slave
i send two bytes for test from master raspberry
when reset mcu it receive ok when i repeat request it receive nothing and rx buffer not changed
i tried checking over run and interrupts and error found nothing
it seem to be time sync problem with master but how it work after reset then stop working without any error
2018-06-15 2:54 AM
there is no time sync, the input clock bits are counted to 8 then the data is latched.
I guess you are clearing the Rx buffer
// initialise by clearing residual bytes in DR
while ((hspi1.Instance->SR & SPI_FLAG_RXNE))
RxSPI = hspi1.Instance->DR;// wait for next Rx
while ((hspi1.Instance->SR & SPI_FLAG_RXNE)) ;
RxSPI = hspi1.Instance->DR; // have new byte //should save to bufferotherwise you may have a poor ground between your SPI device and the F746.
can you check the clock line is going to ground on a scope connected to the F746 ground.?
2018-06-15 6:49 AM
Thanks for replyI tried clean buffer same problemNo problem with groundWhen I use spi polling no DMA it is OK which mean there something with timing I do not know
Sent from Yahoo Mail on Android
On Fri, Jun 15, 2018 at 11:55 AM, T J<st-microelectronics@jiveon.com> wrote:
#yiv5753348846 * #yiv5753348846 a #yiv5753348846 body {font-family:Helvetica, Arial, sans-serif;}#yiv5753348846 #yiv5753348846 h1, #yiv5753348846 h2, #yiv5753348846 h3, #yiv5753348846 h4, #yiv5753348846 h5, #yiv5753348846 h6, #yiv5753348846 p, #yiv5753348846 hr {}#yiv5753348846 .yiv5753348846button td {}
|
STMicroelectronics Community
|
Re: SPI_DMA Slave Receive only after reset
reply from T J in STM32 MCUs Forum - View the full discussion
there is no time sync, the input clock bits are counted to 8 then the data is latched.
I guess you are clearing the Rx buffer
// initialise by clearing residual bytes in DR
while ((hspi1.Instance->SR & SPI_FLAG_RXNE))
RxSPI = hspi1.Instance->DR;
// wait for next Rx
while ((hspi1.Instance->SR & SPI_FLAG_RXNE)) ;
RxSPI = hspi1.Instance->DR; // have new byte //should save to buffer
otherwise you may have a poor ground between your SPI device and the F7
can you check the clock line is going to ground on a scope connected to the F746 ground.?
Reply to this message by replying to this email, or go to the message on STMicroelectronics Community
Start a new discussion in STM32 MCUs Forum by email or at STMicroelectronics Community
Following Re: SPI_DMA Slave Receive only after reset in these streams: Inbox
This email was sent by STMicroelectronics Community because you are a registered user.
You may unsubscribe instantly from STMicroelectronics Community, or adjust email frequency in your email preferences
________________ Attachments : Untitled.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxUj&d=%2Fa%2F0X0000000ayo%2FHGfZ39noQtg1IrebSpb5L0WsE1iS8K6CaLkz3ndLH44&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.