2018-06-16 11:16 AM
Hi,
I'm a little bit confused about adc and vref.
From reference manual
The internal voltage reference (VREFINT) provides a stable (bandgap) voltage output for the
ADC and Comparators. VREFINT is internally connected to the ADC_IN17 input channel. Theprecise voltage of VREFINT is individually measured for each part by ST during productiontest and stored in the system memory area. It is accessible in read-only mode.What exactly it means?
Thanks for your help
2018-06-16 1:22 PM
Hello
zazo.gennaro
,Some MCU families (STM32L4 for example) provide VREFBUF output where you can output stable bandgap voltage to ADC reference via buffer and VREF+ pin.
2018-06-16 4:43 PM
Thanks for help.
On Sat, 16 Jun 2018, 22:22 Tilen MAJERLE, <st-microelectronics@jiveon.com>
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.