2018-06-16 1:57 PM
I would like to use STM32F446MCY6TR in my new device and for me not clear if can the uC STM32F446MCY6TR executed code in time when erasing a part of flash before write some configuration parameters or the core full stop exeucute any instructions until erasing/writing operation will not finish?
Thanks.
#stm32f4-flash2018-06-16 2:31 PM
It basically stalls out by inserting wait-states until complete.
Some STM32 devices support multi-bank FLASH which would allow normal functioning of the opposing bank during write/erase.
You may also put your code, vectors, and irq handlers in RAM, and provided nothing executing touches FLASH you can run real-time code that doesn't stall.
2018-06-16 3:10 PM
I know what some
STM32 devices support multi-bank FLASH I just would like make sure if theSTM32F446MCY6TR not support it as I did not find the information in reference manula, I found only that:
3.5 Erase and program operations For any Flash memory program operation (erase or program), the CPU clock frequency (HCLK) must be at least 1 MHz. The contents of the Flash memory are not guaranteed if a device reset occurs during a Flash memory operation. Any attempt to read the Flash memory on STM32F4xx while it is being written or erased, causes the bus to stall. Read operations are processed correctly once the program operation has completed. This means that code or data fetches cannot be performed while a write/erase operation is ongoing.
Is I am correct that STM32F446MCY6TR which the
devices NOT support multi-bank FLASH?
Thanks.
2018-06-16 5:34 PM
Single bank device
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.