STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_Irda problem : ping-pong communication fails

Posted on April 21, 2017 at 12:03Hi everyone,I'm developing a firmware in which a IR communication protocol is designed. The uC is a STM32F042C6 and I'm using HAL drivers.The protocol should work as follow (infinite loop):1> Receive 1 byte in interr...

Stm32L4 internal temperature sensor measurement

Posted on July 02, 2018 at 22:38Hello, I'm trying to measure the ambient temperature using the nucleo l432kc internal temp sensor . I connect the MCU through the usb to my lapotp. With the code I'm currently using, the output temperature starts at 2...

STM32F103VCT6  USB Communication Disconnection problem

Posted on July 03, 2018 at 09:38I have used CubeMX to generate the USB CDC driver. I connect my board to a PC and the device manager recognize it as: 'STMicroelectronics Virtual COM Port (COM1)', And then the device is connected.- STM32Cube V1.0 Ver...

Description GPIO speed

Posted on July 03, 2018 at 00:09I want to know how can I aware about some gpio speed parmeters in Cube (low - medium -fast -high speed).For example I set cpu on 20Mhz and PinC.1 set as output push pull medium speed. In this state , what's the pin sp...

Calling HAL_Delay while in sleep

Posted on July 03, 2018 at 05:23Hi,What is the expected MCU power consumption / CPU state when calling HAL_Delay() from an ISR triggered while MCU is in STOP mode? 

STM32CubeMX H743ZIT Makefile problems

Posted on July 03, 2018 at 00:08I'm trying to build a simple 'hello world' program on the STM32H743 using the Makefile option and the standard Ubuntu arm-none-eabi-gcc V 4.9.3.  At this stage my program doesn't even do floating point, but it will ev...

Difficulties with the purchase of sdtam 16Mx32 512Mbit.

Posted on July 02, 2018 at 12:53At the moment, almost all the memory chips of such a configuration are discontinued. They were not popular at the time of active sales, and after the end of support for manufacturers - leftovers remained at an inadequ...

STM32F767 External SRAM

Posted on June 30, 2018 at 18:33Hi .I have a custom board with ''stm32f767'' mcu on it and an external sram ''is62wv51216bll-55tli ''.I have two problem first is when MPU is Disable and i have this config :↓  SCB_EnableICache();  SCB_EnableDCache();...

0690X0000060LYpQAM.png
M N by Associate II
  • 3956 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.