STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Set WKUP pin to no push/pull after Standby STM32

Posted on June 25, 2018 at 17:14When I send the device into standby it appears that the WKUP pin is held low. For my application this causes an issue with the Comparator that is in the circuit before the pin. Is there a way to configure the WKUP pin...

STM32L0: wrong address of COMP registers in svd file

Posted on July 02, 2018 at 13:33Hello! I use MDK from Keil and noticed, that the address of the COMPn_CSR registers in the SystemViewer have wrong addresses.I checked the SVD files in the latest STM32L0xx_DFP V2.0.0. The problem is the base address ...

SD CARD STM32L052

Posted on June 22, 2018 at 13:51Hi everybodyI have little trouble about STM32L052 and SD Card reader.I don't have much knowledge about SPI communication in STM and I never used before SPI,FATFS but it seems to complex to me  anyone can help me ? If ...

Mqtt client on STM32F429ZI Nucleo

Posted on July 02, 2018 at 14:32Hello,I am trying to implement mqtt client on my STM429ZI Nucleo.I have initiated TCP / IP stack and it works well.I downloaded the MQTT library from https://community.st.com/external-link.jspa?url=https%3A%2F%2Fgithu...

daw ka by Associate II
  • 1007 Views
  • 0 replies
  • 0 kudos

detect flash is in progress

Posted on July 02, 2018 at 11:26Hi to everyone,I'm working on STM32F411 and I'm wondering if it's possible at the start of a code, detect if a new flash code is in progress to stop the code execution and wait for the flash. This strange problem is d...

DUrbano by Associate III
  • 1203 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.