STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429 SMBus Implementation

Posted on November 15, 2016 at 07:54Dear all,for a project I have to implement a SMBus communication with a battery. I already found the X-CUBE-SMBUS Software but it seems that it is only compatible with F0 and F3 Controllers. I also saw that these ...

STM32F479IIT6

Posted on July 04, 2018 at 12:19we are using STM32F479IIT6 in our design as below,1.USB 2.0 full speed2.Self powered3.As deviceCould you clarify on the following points,1.what is default configuration of OTG_FS_ID(left unconnected,GND or pullup)2.si...

HCD_HandleTypeDef on HS port

Posted on June 28, 2018 at 20:30On STM32F7, the host mode offers 16 channels on the HS port.But in the HAL, the HCD_HandleTypeDef structure contains only 15 items HCD_HCTypeDef.What is the reason for the missing channel ?Is this a bug ?Is this norma...

I-Jet Trace not performing ETM trace.

Posted on July 05, 2018 at 17:13Hi All,         On full paid version of IAR Embedded Workbench I am trying to use I-Jet Trace.After carefully connecting all the wires keeping in mind MIPI20 connections on Nucleo144 STM32F767. I am able to power and ...

0690X0000060CDLQA2.png 0690X0000060CDQQA2.png 0690X0000060CDMQA2.png 0690X0000060CDVQA2.png
A Maq by Senior
  • 1354 Views
  • 0 replies
  • 0 kudos

Wrong Flash Size on STM32F103C8T6

Posted on July 05, 2018 at 16:37I'm just confused by a Board called Blue-Pill in the Community. It has a STM32F103C8T6 installed, but the Flash-Size Readout is 0x20000 and not 0x10000 for 64k as expected. It is also possible to use this Flash.Here i...

Resolved! pwm pin out on nucleo stm32f303k8

Posted on July 04, 2018 at 12:51Hi EveryOne.Hi have a problem with PWM on my Stm32f303k8, nucleo board.Hi searched on this forum, but I not find an answer that solve my problem.So: I need to have a pwm output on PB_1 Pin, and, to do this, I've used ...

STM32L152 Timer10/11 - Compare capture interrupt

Posted on June 26, 2018 at 17:20Hi,I want to use TIM10 or 11 for generating the interrupt when the counter CNT reaches the value stored in CCR1 register (capture/compare). I want NO output  to be generated on output pins. I also want run from intern...

JAN R by Associate III
  • 3479 Views
  • 7 replies
  • 0 kudos

meaning

Posted on July 05, 2018 at 11:54Bonjour tout le mondeJe veux comprendre ce que cette ligne signifie s'il vous plaît?Merci d'avance

Jessy J by Associate II
  • 2048 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.