2018-07-04 3:19 AM
we are using STM32F479IIT6 in our design as below,
1.USB 2.0 full speed
2.Self powered
3.As device
Could you clarify on the following points,
1.what is default configuration of OTG_FS_ID(left unconnected,GND or pullup)
2.since it is self powered,there is no need of 5V supply(VBUS is used for sensing of host connection)
Thanks,
Arun D.
#stm32f479iit6-usb-id2018-07-05 7:05 AM
Hi
arunkumar.devershett
,unconnected.
which covers the most important points that should be taken into consideration when using the USB peripheral embedded inside the STM32 MCUs. Section &39Hardware guidelines for USB implementation -> USB FS upstream port&39 explains the hardware requirements for a correct operation of the USB peripheral in device mode
Khouloud.
2018-07-05 9:20 AM
Hi Khouloud,
I have referred the attached application note however it is not mentioned about OTG_FS_ID, also given snapshot below.
As ID pin is required in OTG applications only, can with go with unconnected.
Kindly help us in getting configuration of OTG_FS_ID in USB 2.0 full speed as a device/peripheral.
Thanks,
Arun D.
________________ Attachments : image001.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxRQ&d=%2Fa%2F0X0000000ay6%2FrVu9PICuS90fAcYxP5gY4TjPP9oU3BNkzzzUMEj8iwk&asPdf=falseApplication note_USB hardware using STM32 MCU.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HxRL&d=%2Fa%2F0X0000000ay5%2FWx7v_OKNehFRTOuSorN2g.JZ8P8sTsyOuwosQnaArAU&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.