STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STemWin

I have managed to get STemWin showing the "Hello World" message on the STM32F779I-EVAL board using CubeMX.The project has FreeRTOS enabled.Maybe it's me not understanding STemWin... but it seems after the screen refresh during the initialization, STe...

TDahl by Associate II
  • 852 Views
  • 0 replies
  • 0 kudos

Is that possible to use SWO without Debugger?

Hi,​My target is STM32L151 (Cortex M3). ​I would like to print data through SWO without a debugger connected to SWD . Is it possible? If it is, should I configure something in the STM32? Thank you for any help!​

Yevpator by Associate III
  • 2706 Views
  • 5 replies
  • 0 kudos

Resolved! STM32L476 measured VREFINT has wrong value

Hello all,I followed the reference manual to determine VDDA for STM32L476VET6, using the VREFINT measured value together with the calibration value using following code: if (HAL_ADC_PollForConversion(&hadc1,100) == HAL_OK) {ADC_measure_VREF = HAL_ADC...

Resolved! STM32L4 ADC1_IN2 and ADC1_IN15

Hi,I am having issue reading ADC1_IN2/IN15. The value return from HAL_ADC_GetValue(0 is either 0 or close to 0. Others seems fine. I do use exactly same function to read. The results are list below as iSense last 2 value 0 0. Is there anything specif...

STM32F4 DMA source/dest address alignment requirements

The RM0090 Reference manual (DocID018909 Rev 10) mentions on p310 that :When the data width (programmed in the PSIZEor MSIZE bits in the DMA_SxCR register) is a half-word or a word, respectively, the peripheral or memory address written into the DMA_...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.