STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Have I found a driver issue?

Greetings, I'm using an STM32L496. I have a peripheral connected to PE11, which I have configured as an interrupt on the rising edge. I have another circuit connected to PA11, which is normally an input. So far no problem. In order to do a sel...

Can we take TIMER2, Channel3 for External clock mode1 for frequency counting upto 5-10 MHZ? Board: STM32F401RE [Nucleo Board], PIN: PB_10 [Timer 2, channel3]

Can we take TIMER2, Channel3 for External clock mode1 for frequency counting upto 5-10 MHZ? Board: STM32F401RE [Nucleo Board], PIN: PB_10 [Timer 2, channel3].In case, yes.. Can anybody provide me refrence or sample code?

SRai.17 by Associate II
  • 1747 Views
  • 4 replies
  • 0 kudos

Stm32l011k4 and Adafruit Sharp memory display breakout

Hello, I am trying to use the STM32l011k4 with the Sharp memory display breakout from Adafruit. I succeeded in clearing the screen but I can't display a pixel on the screen. I always have the same display, probably what the buffer contains. I don't k...

Jean1 by Associate
  • 826 Views
  • 0 replies
  • 0 kudos

STM32F303 OPAMP Timer controlled Multiplexer mode

I'd like to amplify two signals connected to non-inverting input of OPAMP and control which one is currently amplified by TIM1, Channel 6. This technique is described in RM0316 document, chapter 18.3.6 Timer controlled Multiplexer mode.I've set TIM1,...

0690X000006BwyUQAS.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.