STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DFU mode -- Can it be entered with power on?

When I put 3.3V to boot0 and 0V to boot1 and then 0V to NRST,I don't get DFU mode. I have to cycle power withboot0 HI to the MCU to get DFU mode.The docs suggest different. have I misinterpreted the docs?Thanks, John

Jump application bootloader 0x8003000 interrupt not working

hi guys!Can you help me solve that problem:I had write bootloader for stm32F300rct6, program have jump to main application success but interrupt not working. I don't know what is missing? In main application i edit #define FLASH_BASE ((uint32_t)0x080...

TPham.10 by Associate II
  • 2705 Views
  • 4 replies
  • 0 kudos

stm32 c2c portal does not send activation emails

I registered on stm32-c2c.com website but it continue to tell me that it needs to confirm my email. I never got email with confirmation link. When I click "RESEND" button it says "Email successfully sent" but I never got any. It does not allow me to ...

ESava by Associate
  • 868 Views
  • 0 replies
  • 1 kudos

Nucleo-H743 out of stock

Posted on March 15, 2018 at 12:37I wanted to try Nucleo-H743 board to see, if H7 MCU is a good choice for my application. But it seems like there's no vendor that provides the board. I think it has been a while since the board is out of stock. Does ...

M. Jeong by Associate II
  • 4000 Views
  • 9 replies
  • 0 kudos

Programming STM32F401RET6 WITHOUT Nucleo board

I'm trying to find how to program the STM32F401RET6 MCU on a standalone PCB without the development board. The datasheet specifies using JTAG for debugging but does not specify that this could be used for initial programming too. Could anyone help me...

CMead by Associate
  • 1442 Views
  • 1 replies
  • 0 kudos

hidden pins in STM32L0 CAD Symbol and Footprint files

I downloaded "STM32L0 CAD Symbol and Footprint files", open STM32L0x1KUF6.bxl, and converted it to .lbr Eagle CAD file. I opened the file in Eagle and realized that some pins(No.1,5,17) are hidden. why? I'm a beginner of Eagle

YFuku.3 by Associate III
  • 863 Views
  • 1 replies
  • 0 kudos

Stm32F303 Timer1-Prescaler Problem

Hello all,I am using the nucleo Board Stm32F303Ze where I want to trigger the ADCs with Timer1 after 3 or 5 cycles when the Timer is set to 144 MHz. The configuration is done in CubeMX.Generally the triggering of the ADCs and the transmission via DM...

Bench by Associate III
  • 1944 Views
  • 8 replies
  • 0 kudos

interfacing PDM mic with STM32F4

Hi, now it seems I can successfully sample audio data, below is the spectrum of 10KHz tone signal.However, in an acoustically quiet room, the mic can still sample high freq noise, which confused me.Now there are 2 things also confuse me:It seems the ...

J Lee by Associate III
  • 1436 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.