STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI with STM32f429

Hi,I am using an STM32f429 Discovery board with CubeMX and HAL, and have some problems regarding SPI. I am using an DAC which takes data in 24 bit format, 8 control bits and 16 data. I can only select between 8 or 16 bit data, not both. If I try to s...

Matt G by Associate II
  • 5156 Views
  • 11 replies
  • 0 kudos

CAN3 on NUCLEO-F767ZI is not working for me

Posted on July 10, 2018 at 18:30I'm using STM32CubeMX and Keil �Vision V5.25.2.0to program the NUCLEO-F767ZI board.MB1137 Rev BThe init sequence is:static void MX_CAN3_Init(void){  hcan3.Instance = CAN3;  hcan3.Init.Prescaler = 24;  hcan3.Init.Mode ...

B_12159 by Associate II
  • 2013 Views
  • 3 replies
  • 0 kudos

STM32H7 - "dedicated internal audio PLL"

Hi!The datasheet suggests there is a "dedicated internal audio PLL" in the H7. Can you elaborate further on this PLL? I don't see it singled out anywhere. What are the performance specs?Thanks!

UART DMA TX occasional errors

Once a while my Error_Callback() of the UART DMA RX/TX is triggered and I can't make sense out of it.In the HAL_UART_ErrorCallback the values areHAL_UART_GetState(huart) == 32 // HAL_UART_STATE_BUSY_RX HAL_UART_GetError(huart) == 16 // HAL_UART_ERRO...

How to find a Temperature on STM32F303K8

Hi, Everyone.I'm tring to make adc sensor works, to find a temperature.I found AVG_Slope and V_25 in the datasheet: AVG_Slope = 0.0046 V_25 = 1.46And I used V_Ref = 3.0f and N_Bit = 4096fThis is My code (Only for adc_complete conversion)void HAL_ADC_...

How to use SPI3 of STM32F103RCT6 (no have SCK)

Dear AllNice to meet you. At First My english is poor. Please understand me.I want use M95512 (EEPROM) with STM32F103RCT6 SPI3but now I check Oscilloscope SCK, MOSI, MISO. Only work MOSI have signalnow no work SCK.... How to Init. SPI3 Please check m...

NAND memory readback error

Hello,I'm using a NUCLEO-L496ZG-P board together with a Samsung K9F1G08U0E nand module. At the moment i'm testing read write operations. For certain values what i read from page differs from what i've written. For instance if i fill page with rand() ...

Resolved! STM32L4R9 strange behavior when awaking from shutdownMode

Hello,I enter the shutdown mode with the following code statementHAL_PWR_EnableWakeUpPin( PWR_WAKEUP_PIN1_LOW ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN2 ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN3 ); HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN4 ); HA...

s m by Associate III
  • 1153 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.