2018-09-04 1:22 AM
Hello,
I enter the shutdown mode with the following code statement
HAL_PWR_EnableWakeUpPin( PWR_WAKEUP_PIN1_LOW );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN2 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN3 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN4 );
HAL_PWR_DisableWakeUpPin( PWR_WAKEUP_PIN5 );
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF1);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF2);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF3);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF4);
__HAL_PWR_CLEAR_FLAG(PWR_FLAG_WUF5);
HAL_PWREx_DisableInternalWakeUpLine();
HAL_PWREx_EnterSHUTDOWNMode( );If I wake up the system with PWR_WAKEUP_PIN1, I set the GPIO15 from PORTH to high.
I initialized the PORT and GPIO (CubeMX generates the code).
The result is that the system is hanging. If I reset the GPIO to low before entering the shutdown mode, everything is working fine.
Am I missing something? Maybe someone can explain me if I doing something wrong.
Is there any bug know that happens when using shutdownMode on STM32L4+ series?
Thanks.
Solved! Go to Solution.
2018-09-07 9:07 AM
Ok the problem is resolved.
I used inside the interrupt the RTOS message queue and after the reset it was not initialized.
Sometimes it worked, sometimes not, funny.
Sorry for that!
2018-09-07 9:07 AM
Ok the problem is resolved.
I used inside the interrupt the RTOS message queue and after the reset it was not initialized.
Sometimes it worked, sometimes not, funny.
Sorry for that!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.