2018-07-10 9:30 AM
I'm using STM32CubeMX and Keil �Vision V5.25.2.0
to program the NUCLEO-F767ZI board.
MB1137 Rev B
The init sequence is:
static void MX_CAN3_Init(void)
{hcan3.Instance = CAN3;
hcan3.Init.Prescaler = 24; hcan3.Init.Mode = CAN_MODE_NORMAL; hcan3.Init.SyncJumpWidth = CAN_SJW_1TQ; hcan3.Init.TimeSeg1 = CAN_BS1_11TQ; hcan3.Init.TimeSeg2 = CAN_BS2_4TQ; hcan3.Init.TimeTriggeredMode = DISABLE; hcan3.Init.AutoBusOff = DISABLE; hcan3.Init.AutoWakeUp = DISABLE; hcan3.Init.AutoRetransmission = DISABLE; hcan3.Init.ReceiveFifoLocked = DISABLE; hcan3.Init.TransmitFifoPriority = DISABLE; if (HAL_CAN_Init(&hcan3) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}
Ports are PA8 for RX and PB4 for TX.
The CAN buses on CAN1 and CAN2 are working properly.
Behaviour: the init routine jumps through the error handler.
As result CAN3 is not working.
Any ideas?
#can3-on-nucleo-f767zi2018-07-10 5:36 PM
enable ABOM,
do you have a transceiver chip ?
if not, then you need a pullup on the CanRx pin
2018-07-11 4:45 AM
I am using a pullup on the CanRx pin.
As described: I used the same init for CAN1 and CAN2 and there are no problems.
I traced the MX_CAN3_Init routine and found the source of the error:
/* Check Sleep mode leave acknowledge */
while ((hcan->Instance->MSR & CAN_MSR_SLAK) != RESET) { if ((HAL_GetTick() - tickstart) > CAN_TIMEOUT_VALUE) { /* Update error code */ hcan->ErrorCode |= HAL_CAN_ERROR_TIMEOUT;/* Change CAN state */
hcan->State = HAL_CAN_STATE_ERROR;return HAL_ERROR;
} }I traced the code and found, that the routine is always terminated by timeout.
It seems for me, that the CAN controller stays in sleep mode.
Is there a known bug in silicon?
2018-09-10 5:59 AM
Now it is fixed:
Using
CAN1 PB8 and PB9
CAN2 PB5 and PB6
CAN3 PA8 and PA15
Important:
Bridges on the backside have to be soldered as follows:
SB115: close
SB169: open
factory default is: SB115 open, SB169 close
so you have to solder the 0-ohm-resistor to SB115 position
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.