STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer Clock division has no effect

HiI was reviewing my code and I wanted to change some timer configurationSo I use a STM32F727 @216MHz with all clock periph at max speed.I use the following init (generate by cube) to configure TIM2 to get a 1 µs based timer htim2.Instance = TIM2; ...

Resolved! which one is better and easy to understand STM32F0308 Value Line Discovery vs STM32F0308 Value Line Nucleo

i am beginner with stm32 so please suggest which one is better or any other low cost module following are link 1) http://www.dnatechindia.com/Development-Board/STM32-development-boards/STM32F0308-Nucleo.html2) http://www.dnatechindia.com/Development...

prasad1 by Associate II
  • 2290 Views
  • 5 replies
  • 0 kudos

Resolved! HSE of STM32F373RC is not working

Hello.My MCU does not work. I guess it is oscillator problem.- PF1 pin of STM32F373RC is low even though 3.3V power is supplied to MCU, so 8Mhz oscillator does not work. - The oscillator has internal capacitors and part number is "CSTNE8M00G550000R0"...

Diget by Associate II
  • 3143 Views
  • 8 replies
  • 0 kudos

Resolved! Flash page erase operation never completes

I'm trying to erase a single page of flash memory at 0x0800F800 (on a 64kB STM32F103C8T6) by using the following code, which runs from RAM:while(FLASH->SR & FLASH_SR_BSY); FLASH->CR = FLASH_CR_PER; FLASH->AR = 0x0800F800; FLASH->CR |= FLASH_CR_STRT; ...

SAnuf by Associate
  • 2418 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.