STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flashing problem in STM32F207

I try to flash using st-link v2 but it show the error message. In my design I cant able to access the Boot 0 and Boot1 pins so no possibility to go for DFU mode.Please give any solution to flash using st-linkV2 kmani@kmani:~$ st-flash erase2018-09-25...

Resolved! DBGMCU in RM0433 has wrong offset for DBGMCU_APB4FZ1.

Hello,In the RM0433 (rev 3) the DBGMCU_APB4FZ1 offset is incorrectly marked in the detail section.It is 0x04C and should be 0x054.The register summary is correct. But if somebody is using the detail section - can make an error.BTW: What does the LS s...

How to connect SDMMC with 48-Pin STM32L431CC ?

On this site is stated that the STM32L431CC 48-Pin Package has an SDMMC interface... https://www.st.com/en/microcontrollers/stm32l431cc.htmlBut when have a closer look to the HW Manual, the AF functions are only avail at PORT C and PORT D... witch im...

Optimizing Current Consumption for STM32L151CBU6

Hi All,I am using the STM32L151CBU6 MCU under battery operation with 32MHz and 32.768kHz crystals. On running it on STOP Mode with low power regulator using the API:HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON,PWR_STOPENTRY_WFE)The current consumpt...

KPrad.14 by Associate
  • 1195 Views
  • 2 replies
  • 0 kudos

STM32 and Apple MFi

Posted on December 04, 2013 at 11:08Dear allI have developed a USB MIDI device product based on STM32L151.Now I would like to make this product working with Apple MFi protocol.I was wondering if I could find somewhere some inputs about MFi source co...

jerome2 by Associate II
  • 2440 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.