STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read multi channels ADC using DMA

hi everyone. my project uses STM32f407, i read 4 channesl analog by ADC1 and using DMA .when i debug the program, i can only read the first analog value... please help me. bellow this is my program#include "stm32f4xx.h" #include "stdio.h"   GPIO_Ini...

dthan.17 by Associate
  • 639 Views
  • 0 replies
  • 0 kudos

STM32H753 and STM32H743 (the difference)

I need a development kit/board with STM32H753 MCU. I find similar - https://www.st.com/en/evaluation-tools/nucleo-h743zi.html  And decide to solder STM32H753 instead of STM32H743.I saw STM32H753I-EVAL, but it is too expensive. What is the difference ...

VK.17 by Associate II
  • 10172 Views
  • 8 replies
  • 0 kudos

FATFS API

hi, i have the HAL driver for sd card and fatfs software module but i can't understand the mechanisms that both hal and fatfs api's, it's all confused me. stuck here unable to move forward.@Community member​ @Community member​ 

Ark1 by Associate II
  • 5587 Views
  • 9 replies
  • 1 kudos

Full duplex USART example for STM32F722

Posted on February 15, 2018 at 15:52Hello.Ive worked with the two boards comm DMA sample program and it works but it only works half duplex.The flow is:Init UART handle,Transmit dma wait for tx interupt callbackreinitalize UART handleRecieve dma wai...

Using the SPI module during the receiving data via DMA

Hi everyone,I'm using the DMA to receive the data from external flash via DMA. Can the SPI module transmit data while receiving from external flash at the same time? Or will it block this transmitting until completing the receiving? Or can simultaneo...

STM32F103 - CubeMX DFU

Hi,I couldn't find online a working bootloader implementation of STM32f103C8 based on generated files from CubeMX, i've started porting the F4 DFU to F1, there are two applications: 0x08000000 - DFU Bootloader0x08008000 - ApplicationJump between the ...

Resolved! Another funny typo, in the USART chapters of RMs

In USART block diagram figure, "f" in "Transmit shift register" is missing, giving it a whole lot different meaning... ;)Besides this, the arrows from both "shi(f)t registers" to their respective data registers have incorrect direction. The LPUART ch...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.