STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help with X-CUBE-SPN2 for IHM02A1

Posted on December 01, 2017 at 21:47Has anyone used the IHM02A1 and got either the project files or the pre-compiled binary and hex files to work? If so, could you please tell me if you did anything to get them to work or did they simply work out of...

DMA multi-using problem

Posted on October 24, 2017 at 11:30I use STM32F103, DMA1->CH6USART2 RX and TIM3 TIM3_CH1 both can use this channel.If only USART2 RX or TIM3 TIM3_CH1 to use this channel,it is ok!but how to multi use for two request?thank you very much.

STM32F030C8T6 DMA USART CHANNEL REMAPPING QUESTION

Hi everyone: As a title,I use dma Usart Rx for DMA1 Channel 3,but at the same time, I also use Spi Tx for DMA.So , I must remap Usart Rx from DMA1 Channel 3 to DMA1 Channel 5.I try to use this function SYSCFG_DMAChannelRemapConfig(SYSCFG_CFGR1_USAR...

Help required with porting from STM32F767ZI to STM32F779NI

I have code that runs on the NUCLEO-F767ZI kit and have recently obtained the STM32F7779I-EVAL kit. My program is very simple, it does not do any IO (yet), so I (perhaps naively) thought that just changing the processor type in my IAR Embedded Workbe...

KDuff.15 by Associate II
  • 1526 Views
  • 2 replies
  • 0 kudos

DMA abort with JPEG output

The JPEG decoder output DMA aborts after a few iterations. In the function HAL_DMA_IRQHandler, the hdma->state shows that it is in abort state. What can cause the JPEG output DMA to abort?I am using the HAL JPEG decoder on a stm32F779, the JPEG decod...

MNour by Associate
  • 644 Views
  • 0 replies
  • 0 kudos

Resolved! How/ Where can i download stm32 cube mx version 4.21?

I am working with SD card in SDIO mode. The current version of cube mx i.e, 4.27 is not working. Some people in the community posted that after version 4.21 SD card issue is persistent. so i would like to download 4.22Youtube link I have followed: ht...

Apill by Senior
  • 1058 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.