2018-10-08 3:37 AM
In USART block diagram figure, "f" in "Transmit shift register" is missing, giving it a whole lot different meaning... ;)
Besides this, the arrows from both "shi(f)t registers" to their respective data registers have incorrect direction. The LPUART chapters and the older STM32's chapters got this one right.
This appears in several 'F0, 'L4, 'F7 RMs.
(This one spotted by @jaromir sukuba )
JW
Solved! Go to Solution.
2018-10-09 5:57 AM
@Community member , yes both issues are logged :)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-10-08 4:00 AM
Or perhaps a frustrated employee ... ;)
2018-10-08 9:40 AM
Hi Jan,
This typo (propagated because of copying the wrong block diagram) is tracked internally to be fixed in all impacted reference manuals.
Thanks for highlighting it.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2018-10-08 9:44 AM
Amel,
Please note that I am talking not only about the typo, but also the direction of the arrows (which are still wrong in the diagrams where the typo was already fixed).
Jan
2018-10-09 5:57 AM
@Community member , yes both issues are logged :)
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.