STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART4 on STM32F407 not receiving data

static void MX_UART4_Init(void) {   huart4.Instance = UART4; huart4.Init.BaudRate = 9600; huart4.Init.WordLength = UART_WORDLENGTH_8B; huart4.Init.StopBits = UART_STOPBITS_1; huart4.Init.Parity = UART_PARITY_NONE; huart4.Init.Mode = UART_...

GScot by Associate II
  • 2179 Views
  • 5 replies
  • 0 kudos

STM32CUBEMX with Discovery F411VE

Hello after installing the latest version of CUBEMX(4.27) and generating a default project for my STM32F411VE Discovery board by choosing the option to initialize all the peripherals in their default mode it ended up not working. After some debugging...

I2C Slave

when i configured my stm32 board as master then i transmit data but in slave mode it does not..i even tested the i2c example provided by Cube MX ,there also i can only transmit data in master mode,but not in slave mode...any idea please?

0690X000006CA8uQAG.png
asim khan by Associate III
  • 1213 Views
  • 1 replies
  • 0 kudos

Send Data using ESP8266 and STM32F407

I am using STM32F4 discovery board. Some sensors data which are gathered by different sensors is saved on an SD card. Now I want to transfer these .txt files to an FTP server. I am not able to send the files as packages, or i m not sure how.  Seeking...

VVerm.0 by Associate II
  • 772 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.