2018-10-10 1:41 AM
I'm working with a STM32L082 (CMWX1ZZABZ-091) and I can not get an accurate value of VRef (ADC_IN17).
This is important because the device is battery powered.
I am using the VREFINT_CAL (0x1FF8 0078 - 0x1FF8 0079) but there is an error of about 100mV.
I have also noticed that I have to wait about 10 mseconds to have a more sensible value but the specifaction is less.
The ADC is working fine with the external inputs but I need this reference to get an absolute value.
Thanks in advance
2018-10-10 5:48 AM
Do you calibrate before using ADC?
Do you use an adequate sampling time?
Is the reference (VDDA/VREF+) stable enough?
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.