Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi good people. I would love to try a display connected to my stm32F411RE. But I cant find any product. Do you know any? thx a lot. Greetings. Jan
I am trying to run the S2-lp SDK example project on truestudio but I am running in so many errors. one of them is that the yfuns.h file is not even the directories.
Dear All,Currently we're using STM32F030CC micro controller to make a programmer which will program STM32F030CC serially via UART Bootloader commands.First we verified / noted the response of every command by sending each command via serial monitor.T...
Hi, I need to interface STM32F7 with a Bluetooth chipset that supports HCI interface over UART/USB. I would like to know if STM32CubeMX provides such a library or is there any other library available that can be used ? Any direction in this regard ...
I've modified the AT-command example from the X-CUBE-SFOX package to add another serial interface as a command link.Now you can enter AT-commands via LPUART1 connected to terminal program on PC or send them from another CPU via USART1 and forward the...
Please tell me how to disable the DFU USB in application code.
How to disable the low power mode of stm32l072 controller.
I've got a few problems when creating a simple project using STM32CubeMX :1) using all the default setting by STM32CubeMX and clicked YES to "initialize all peripherals with their default MODE", the LED ports were default to input mode ! Weird ! If s...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.