STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F042: External clock and clock output

As described before (https://community.st.com/s/question/0D50X00009sWdDqSAK/stm32f042-bootloader-activation) I want to use 2 STM32F042 as CAN controller. So far I planned to use the internal HSI RC oscillator, but a +-5% tolerance seems critical for ...

0690X000006CHJZQA4.png 0690X000006CHJeQAO.png
harald by Associate III
  • 1978 Views
  • 4 replies
  • 0 kudos

Issue with PA2 and PA12 pin in L432KC Nucleo

I'm using a reflective sensor to measure speed. In my PCB, I wrongly connected PA12 to the output of the sensor. I actually needed PA2 to use it as TIM2_CH3. So I jumped PA12 and PA2. This pin is pulled up to 3.3V with a 10K resistor. With no sensor ...

xpp07 by Senior
  • 1190 Views
  • 1 replies
  • 0 kudos

How to use PA15 on STM32F302RD?

Hey,I can't access PA15 with the STM32F302RD µC. It's obv used for JTDI but it's possible to change this mode (if I can trust the reference manuel). With the "flexible SWJ-DP pin assignment" I have to change the mode to "JTAG-DP Disabled and SW-DP En...

External (Timer) trigger for regular ADC channel

Hi everyone!So as the title suggest I would like to get some help for my STM32F303 Microcontroller.In the application Timer1 is used to turn an external pin ON and OFF at a constant frequency, while ADC4 is used to read some feedback with the same fr...

SzIsti by Associate II
  • 2707 Views
  • 5 replies
  • 0 kudos

problem with dfuse

Posted on August 12, 2011 at 10:20Hi,    I am currently developing a PC application for STM32 using Inemo board.The PC application will be able to upgrade the firmware of the STM32 using Dfu mode. Iam using Visual studio Vb.net for the PC side appli...

Resolved! What is the reset value of GPIOx_MODER?

According to RM0433 rev 5 section 10.4.1, the reset values are 0xABFFFFFF for port A, 0xFFFFFEBF for port B, and 0xFFFFFFFF for all the others. This appears to agree with the bits shown in the register table at the end of the chapter. However, in the...

CHead by Associate III
  • 1157 Views
  • 2 replies
  • 0 kudos

STM32 - ATA read/write

Well, i need to read data from the hardware that uses ATA interface, my mcu is stm32f407, all is came in my mind is to make software implementaion by bitbang the pins, but ATA has 16 bits data interface, therefore ill need to bitbang each pin connect...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.