STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unknown Usb Device

HiI configured Usb HID Device libraries for my stmF042k..but windows says Usb device not recognised. since F042k dont have a dedicated user usb,so here is my scheme i connected a usb cable to my stm..i left the power cable open because i am not sure ...

0690X000006CGVeQAO.jpg
asim khan by Associate III
  • 878 Views
  • 0 replies
  • 1 kudos

STM32H743ZI : I can not do a TCP/IP Socket communication

Hello,I try to do a connection via TCP with LWIP/FreeRTOS activated (ioc file joined)For testing i use telnet command and I am unable tio pass the "accept" function.Here the simple piece of code: int sock, newconn, size; struct sockaddr_in add...

eymarf by Associate II
  • 870 Views
  • 0 replies
  • 0 kudos

STM32L4R7ZI SDMMC clock polarity wrong?

HelloI have tried to run a microSD on STM32L4R7ZI and run code from CubeMX 4.26.1 to access the microSD card. According to SDCard Physical Layer spec the card clock should have a rising edge to signal a valid bit clocked into the card. But STM32L4 ge...

0690X000006CAlmQAG.png 0690X000006CAlrQAG.png

Get data from ADC

Hello,My aim is to get data from two ADC channels in order to extrat data into a file. I want then to analyze data with Matlab.For now I achieve to see the two signals in my debugger but I can't manage to extract them from there.I am using a Nucleo F...

STM32F105RB and correct way to start from a new user perspective

Hi all!I'm starting a new application concerning the driving of a small stepper motor by means of the L6480 driver, I'm also new with the ST software toolchain, so I kindly ask to be patient if some question may be obvious from some certain point of ...

FF1 by Associate III
  • 831 Views
  • 2 replies
  • 0 kudos

STM32L4+USART+Rx+HAL-------Distortion of received data

Hello Everyone,I am using Nucleo-32 board in my project. I am programming USART to receive 10 character data and then transmit this 10 character data back. Problem that I am observing is that if accidentally 11 character it is suppose to display erro...

Find MCU by supported Debug/Trace facility

Hallo all,where can I find an overview on which trace block like SWV, ETM or ETB is implemented in the different STM32 MCUs?Currently I am looking for one supporting ETB for evaluation purposes.Kind regardsStephan

SHoff by Associate
  • 1389 Views
  • 2 replies
  • 0 kudos

Resolved! UART Oversampling 8 and 16

STM32 experts,I bought 2xNUCLEO-F042K6 for testing purposes. Reference manual says that uart speed at oversampling 16 is 3mbit/s, for oversampling 8 is 6mbit/s.Here is my working configuration. I send 100 bytes data at 3mbit/s and oversampling 16 fro...

John Doe1 by Associate III
  • 6775 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.